107002 | tof640-20gm_850nm | (Revision 07 or newer is recommended) |
107002 | ES-TOF | (Revision 07 or newer is recommended) |
This is exclusively a producer update – the camera does not need to be updated to profit from the extensive improvements.
Interest in 3D applications and demand for 3D cameras are on the rise – and the advancement of the Basler ToF Camera is also in full swing. The newly launched software package (Version: 1.2.0) for the Basler ToF Camera includes the following new features:
The software package is available for the following camera modules and is ready to download on the website :
107002 | tof640-20gm_850nm | (Revision 07 or newer is recommended) |
107002 | ES-TOF | (Revision 07 or newer is recommended) |
This is exclusively a producer update – the camera does not need to be updated to profit from the extensive improvements.