Your browser is out of date. It may not display all features of this websites. Learn how to update your browser.

OK
Start configuring your vision system now Webshop
7 Jun 2022

New: Hardware Trigger in Basler blaze 3D ToF Camera

New: Hardware Trigger in Basler blaze 3D ToF Camera

In the course of the latest update, we have equipped our 3D Time-of-Flight camera blaze with the Hardware Trigger feature. In contrast to triggering via software settings, with the hardware trigger the image acquisition and exposure are started by an electrical signal, triggered--for example--by a programmable logic controller (PLC) or a light barrier. This electrical signal is fed directly to the trigger input, where it triggers the exposure with virtually no delay. Thanks to this low latency, image acquisition can be controlled even more precisely.

"Frame active" is another new functionality of the blaze 3D camera's new digital output. In a multi-camera system, this output can be used as a trigger input for a second camera. If more than two cameras are used, "Frame active" can be used to cascade the interaction of all cameras. This ensures that all cameras trigger one after the other seamlessly and without any loss of time, without interfering with one another.

For applications that require precise synchronization of image acquisition, such as picking tasks on conveyor belts, the hardware trigger is a valuable feature.

Want to learn more about these and other functionalities of the Basler blaze 3D ToF camera?

Meet our blaze camera

Our sales team is happy to answer any further questions you might have.

You have questions?
We have the answers!

Our Sales and Technical Support experts are avaiable to advise you on all aspects of Basler computer vision components and solutions.

Contact us

Back to Webshop