Your browser is out of date. It may not display all features of this websites. Learn how to update your browser.

OK
Start configuring your vision system now Webshop

Current News

Filter

There are 50 elements available for filtering.

There are  0  results matching your filter criteria.

Show Filter
Reset filters

Sorry, there are no results for the selected filters.

There are 50 elements available for filtering.

There are  0  results matching your filter criteria.

09.11.2022

Basler Presents Innovative Vision Solutions for Medical & Life Sciences at Healthcare Expo 2022

At the upcoming Healthcare+ Expo 2022 in Taiwan, Basler will be presenting our latest vision product portfolio as well as showcase new vision solutions for medical & life science applications. more

02.11.2022

VisualApplets 3.3.2 - New Attractive Licensing

With VisualApplets 3.3.2 you get the full power of VisualApplets for your FPGA graphical programming within a single license. more

18.10.2022

pylon 7.2 with Even more pylon vTools

Try out the new pylon 7.2 to get even more pylon vTools with extended licensing options and Linux ARM support, and a new Static Defect Pixel Correction feature. more

04.10.2022

Improved Lead Times for Many Products

Supply chain challenges in the vision industry have been tough on all of us. While the overall situation is still difficult, Basler is happy to announce that lead times for many of our products have improved significantly. more

21.09.2022

Vision Compatibility for New NVIDIA Jetson Orin Nano Edge AI Platform

Basler Add-on Camera Kits with 5 and 13 MP will also be supporting the new NVIDIA® Jetson Orin™ Nano system-on-modules (SOMs), which have set a new baseline for entry-level edge AI and robotics and are scheduled to be available in the beginning of 2023. Add-on Camera Kits are ready-to-use vision extensions that include an adapter board, camera, lens, and cables. more

12.09.2022

Porting Guide: Simplified integration of dart BCON for MIPI cameras into Yocto-based embedded systems

Our new Porting Guide on this topic step-by-step describes how to integrate Basler dart cameras with MIPI CSI-2 interface into platforms based on Yocto®. It is designed for the NXP® i.MX 8M application processor series and is thus relevant for system-on-module manufacturers or system integrators who want to quickly and easily add vision to their systems. more

09.09.2022

pylon GStreamer Plug-in for Basler Cameras

With pylon GStreamer for media applications such as streaming and video editing/playback we provide an open-source plug-in for the GStreamer multimedia framework. This allows all Basler cameras to be used within the GStreamer framework. more

06.09.2022

Higher Frame Rates: The dart Goes Full Steam for You!

The extensive dart camera product range continues to grow. With twelve new USB 3.0 models, we are expanding your choices with two 2nd generation Sony Pregius sensors. The camera provides frame rates up to 525 fps, becoming even more versatile in challenging installation environments. more

09.08.2022

Mounting Bracket for blaze RGB-D Solution Now Available

The new mounting bracket for the blaze makes your RGB-D solution even easier. Combine the RGB data of a Basler area scan camera like the ace 2 with the depth data of the Basler blaze camera and get 3D point clouds in true color. more

03.08.2022

Improving Automotive Assembly Line Efficiency with 3D Robot Vision Powered by Basler

Basler vision components, mounted onto a robot arm, are integrated into Chinese company Alsontech’s 3D robot vision systems, which are widely used in automotive automation. more

26.07.2022

Basler To Present New and Upgraded Vision Solutions at The Upcoming Taipei Automation

This August, Basler Will Present New Highlights From Our Product Portfolio As Well As Showcase New Vision Solutions For Industrial Automation At The Taipei Automation Exhibition. more

19.07.2022

pylon 7.1 - The Best Performance for 5 and 10 GigE! 

With pylon 7.1 you get the best performance and usability for your 5 and 10 GigE Vision setup. more

05.07.2022

Boost Your Speed with New CXP-12 Solutions

For applications with high frame rates, we introduce eight new models of the boost camera series with Sony sensors: With one or two CXP-12 channels, resolutions from 2.8 to 12 MP and frame rates up to 400 fps, they are ideal for inspecting electronic devices and semiconductors as well as for applications such as 3D AOI/SPI systems, intelligent transportation systems (ITS) or fast process automation, such as for sorting tasks. more

28.06.2022

Improving Mini-LED Production Efficiency and Yields with Basler’s Vision Components

In the AOI systems for the quality inspection of mini-LED units, the Chinese company Mento relies on Basler's high quality vision components with customized designs to deliver results. more

09.06.2022

Basler pylon vTools: Image Processing Modules for the New pylon 7

Intelligent structure recognition, precise object positioning or robust code recognition: design, test and flexibly integrate into your own application in one go with camera control and image acquisition! Always perfectly matched to Basler's camera portfolio. Test it now free of charge! more

07.06.2022

New: Hardware Trigger in Basler blaze 3D ToF Camera

Precisely controlled image acquisition with significantly reduced latency: thanks to the new Hardware Trigger feature, you can achieve real-time behavior for 3D image acquisition in your application. more

31.05.2022

Basler Presents New Vision Solutions For The Semiconductor Industry at Semicon SEA 2022

At the upcoming Semicon Southeast Asia Exhibition in June 2022, Basler will present new highlights from its product portfolio as well as showcase new vision solutions for electronics applications. more

31.05.2022

Basler at Nepcon Thailand 2022 with Computer Vision Solutions

Basler will present our current product portfolio for electronic manufacturing at the upcoming Nepcon Thailand Exhibition in June 2022. more

19.05.2022

Basler Reaches Agreement on the Acquisition of the Distribution Business of Advanced Technologies

With the acquisition of the distribution business of Advanced Technologies, Italy, Basler intends to further expand its direct business in Europe. Both companies are looking forward to expand and strengthen the development of Basler AG's sales activities in the EMEA region. more

13.05.2022

Best Managed Companies Award – A Triple Success

Three times in a row: The Basler Management Board and the entire staff are proud to again receive the Best Managed Companies Award. It honors excellently managed companies with strategic foresight, innovative strength, and a sustainable management culture. more

10.05.2022

pylon Camera Driver for Robot Operating System 2 (ROS 2) 

Basler customers can now develop robotics applications on the Robot Operating System 2 (ROS 2). Download the software package "pylon-ROS-Camera" for free. more

09.05.2022

Basler blaze: Now with Dual Exposure HDR

Thanks to the newly integrated High Dynamic Range (HDR) feature, both low and highly reflective parts of a scene can be precisely detected and processed from both very bright and very dark areas. The HDR feature is part of the latest blaze firmware update. The release is available for free download. more

03.05.2022

Computer Vision Solutions for Medical & Life Sciences

From now on, we offer our solution portfolio for applications in the Medical & Life Sciences field. Solutions consist of hardware and software components as well as the development services of assembling a fully consistent system. Benefit from our expertise derived from already-implemented projects in automated microscopy, ophthalmology and medical imaging. more

03.05.2022

Basler and i2S Announce Joint Venture in Distribution Business

Computer vision expert Basler and French machine vision specialist i2S announce plans for Basler to acquire a stake in i2S and establish a joint venture. Basler thus would expand its direct business in Europe. more

26.04.2022

Boost Your Resolution: Our CXP-12 Vision System for High Resolution Applications

The perfect team for high resolution: combining a high-resolution boost camera featuring sensors from onsemi's XGS series and specially developed Basler F-mount Lenses ensures optimal sensor performance for the sharpest images. more

19.04.2022

Basler to Showcase at KIAE 2022 : More New Vision Possibilities

Basler will present innovative solutions that moves the vision industry forward at the delayed Kaohsiung Industrial Automation Exhibition 2022 in May. more

12.04.2022

Don’t Miss Critical Product Changes

Keep your equipment in top shape—sign up today for product updates. Receive the latest Product Change Notifications (PCNs) delivered directly to your inbox. more

12.04.2022

The New VisualApplets 3.3.1 Is Available Now!

Discover the integrated development environment for real-time applications on FPGA processors in image processing. VisualApplets allow FPGAs to be programmed via data flow models on a graphical user interface. more

11.04.2022

Basler CXP-12 Components Ensure Perfect Paint Quality for Vehicles

In a system for testing the surface quality of coatings, the Spanish company Eines Vision Systems relies on Basler's high-quality CXP-12 components from a single source. more

05.04.2022

Basler Reports Strong Annual Result for 2021

Despite some adversities, Basler looks back on a very successful fiscal year 2021: Sales grew by 26 %, orders by 78 % to new record values. more

04.04.2022

Lens Selector Upgrade

Our Lens Selector with new features: Find lenses that fit your sensor and the lens that best fits your technical requirements or has the best price/performance ratio. more

29.03.2022

Warehouse Automation with Basler Vision Solutions 

Warehouse automation solutions from Basler make your logistics faster, smarter, and more efficient. Our perfectly matched products offer reliable vision solutions at the best price/performance ratio. more

07.03.2022

CXP-12 Inspection of Electronic Components

Basler's CXP-12 image processing solutions are used in the quality assurance of various electronic components. boost cameras with a large depth of field (telecentric lens) and those with high resolutions including a large field of view are ideal for imaging defect inspection of CMOS image sensors and brightness inspection of display panels. more

24.02.2022

New in Basler’s 3D Portfolio: Stereo Cameras with Modular Application Software for Vision-guided Robotics

Following the blaze Time-of-Flight camera, Basler is expanding its 3D portfolio with an easy-to-use and industrial-grade stereo camera series with modular application software for various vision-guided robotics applications. This is how you get your robots to perform at their best! more

24.02.2022

Basler Asia Expands with a Second Location in Singapore

Basler Asia is expanding with a second location in Singapore, sending a clear signal for our ramped-up growth. more

22.02.2022

dart – Small Size, Best Image Quality, Great Price

The dart USB 3.0 board level camera comes in six new models that have it all. As one of the first in their class to be equipped with a Sony IMX548 BSI Pregius S sensor of the 4th generation, the small but powerful cameras master big tasks with the best image quality. more

08.02.2022

Dust Protection+: Upgrade of the MED ace Feature Set

The “+” makes all the difference in the new MED Feature Set Dust Protection⁺ for our MED ace camera series: higher cleanliness, better image quality, same price. We accomplish this thanks to such processes as additional and stricter tests of selected components for impurities during assembly. more

07.02.2022

Which CMOS Sensor Is the Right One for My Application?

The IMX models of Sony's four CMOS sensor generations have one thing in common: they are true powerhouses of modern CMOS technology. Our Vision Campus article explains how the individual generations are similar and in which important properties they differ--so that you can find the sensor that best meets your requirements from the IMX variety of Pregius, STARVIS and Pregius S. more

07.02.2022

Pick-and-place Robot in an Industrial Bakery

For the packaging line of an industrial bakery, KINE Robotics relies on the blaze 3D Time-of-Flight camera to enable automated picking of baked goods with a 3D vision-guided robotics system. The customer benefits from the improved allocation of employee resources as well as the increased throughput of goods. more

31.01.2022

Basler Joins 5G Alliance for Connected Industries and Automation

As the first camera manufacturer in the member circle, Basler supports the platform in bringing together the areas of Information Technology (IT) and Operational Technology (OT) and establishing 5G in the industrial sector. more

14.01.2022

3D Bin Picking Solution for Metallic and Shiny Objects

Italy-based software firm Euclid Labs has developed Nak3D, an industrial 3D vision solution specifically designed for scanning challenging shiny objects. The stereo vision system is composed of two Basler ace USB 3.0 cameras and a laser line. more

Show more
Back to Webshop