Your browser is out of date. It may not display all features of this websites. Learn how to update your browser.

OK
Careers | Investors

Press Releases

Filter

There are 15 elements available for filtering.

There are  0  results matching your filter criteria.

Show Filter
Reset filters

Sorry, there are no results for the selected filters.

There are 15 elements available for filtering.

There are  0  results matching your filter criteria.

21.01.2020

Basler at embedded world 2020: Innovative Embedded Vision Solutions in Cooperation with Strong Partners

Cloud connections, AI and machine learning: solution provider of vision systems presents product innovations at booth 2-550 more

14.01.2020

New Products in the ace 2 Camera Series: Models with Sony CMOS Sensors with Resolutions of 5 MP and 8 MP

Basler is expanding its portfolio of the recently introduced ace 2 camera series with 16 additional models featuring the Sony IMX334 CMOS sensor. The new cameras are complementing the ace 2 series with resolutions of 5 and 8.3 megapixels. more

07.01.2020

Basler releases first camera module for NXP’s i.MX 8M Plus applications processor

As a Preferred Vision Partner, Basler worked jointly with NXP to develop a high-performing vision system for Machine Learning (ML) edge computing applications that leverages the full potential of both the camera module and the SoC. more

26.11.2019

Basler Expands Portfolio for NXP’s i.MX 8 Processor Series

With new development kits for a variety of processors within NXP’s i.MX 8 processor series, Basler offers its customers tailor-made solutions in cooperation with well-known SoM manufacturers. more

17.10.2019

Basler AG and drag and bot GmbH: Joint Integration Project Facilitates Robot Programming

In a joint project between Basler AG and drag and bot GmbH, Basler's 2D cameras were integrated into the graphical robot programming software drag&bot. Thanks to the integration of the proven Basler pylon Camera Software Suite into the drag&bot software, it is now possible to intuitively operate Basler 2D cameras in robotic applications. A second result of the cooperation is an improved driver for Basler 2D cameras for the Open Source Framework ROS. more

18.09.2019

Basler Life Sciences Vision Days 2019 @COMPAMED / MEDICA

For COMPAMED / MEDICA, Basler AG presents its high-performance portfolio for Medical & Life Sciences applications: from Basler MED ace and Embedded Vision Solutions to Vision Systems for Deep Learning. more

28.08.2019

Now Available – Design-in Samples of the Basler boost Camera and Basler CXP-12 Interface Card

The new CoaXPress 2.0 (CXP-12) evaluation kits are now ready for orders. The kit consists of a Basler boost camera, the corresponding Basler CXP-12 interface card and the CXP-12 accessory starter kit for a faster and less expensive evaluation phase. For the activation, the pylon Camera Software Suite is an impressive SDK for the camera as well as for the interface card.. more

06.08.2019

Basler Embedded Vision Solutions Now Also Available for NXP’s i.MX 8 Applications Processor Series – First Products Launched

Two new dart camera modules and Add-on Camera Kits provide an ideal starting point for adding image processing to NXP’s i.MX 8 applications processors. more

16.07.2019

Basler Expands 3D Camera Portfolio with blaze

New, universally usable Time-of-Flight camera with high precision for cost-efficient 3D imaging in real time. more

10.07.2019

Now even more models in series: Basler MED ace USB 3.0 cameras with 9 MP and 12 MP resolution

Camera manufacturer Basler is starting series production of additional models in its MED ace product line, which is specifically designed for the Medical & Life Sciences area. All MED ace camera models are produced and distributed according to ISO 13485:2016. Unique MED Feature Sets respond to customer needs in this market. more

11.06.2019

Now in series production: The award-winning Basler dart BCON for MIPI Development Kit with Qualcomm Technologies SoC

The award-winning Basler dart BCON for MIPI Development Kit with powerful industrial Qualcomm® processor is now in series production. The Basler dart with MIPI interface enables lean embedded vision systems without compromising image quality and expands Basler's technology portfolio for embedded vision solutions. more

27.05.2019

Basler ace 2: Next Generation of the ace Camera Series with Unique "Beyond" Features

Basler launches the next generation of its ace camera series: ace 2. An optimized hardware design, the latest CMOS sensors and powerful features such as Compression Beyond, Pixel Beyond and PGI ensure higher frame rates, reduced data volumes and superior image quality. The new ace 2 series kicks off with four models each in the ace 2 Basic and ace 2 Pro product lines. They feature Sony's IMX392 sensor, offer 2.3 megapixels resolution, and deliver up to 160 frames per second. more

09.05.2019

Business figures for the first three months of 2019: Basler closes the first three months of 2019 along its sales and result forecast

BASLER AG, the leading global manufacturer of industrial cameras, is presenting today final figures for the first three months of 2019. more

16.04.2019

Unique in the market: Basler launches intelligent lighting solutions

Basler launches intelligent, easy-to-install and cost-effective lighting solutions. Depending on the requirements of the vision system, customers can choose between a flexible and an easy approach. more

21.03.2019

Basler Reports Business Figures for 2018: Company Confirms Annual Result and Gives Forecast for 2019

Company achieved sales of 150 million euros and a pre-tax margin of more than 16% with a high increase in headcount more

Show more