Shape Centroid Algorithm for Real-Time Industrial Vision
When only position data is needed, sending full images to a PC wastes time and bandwidth. Our customized camera solution preloads the Shape Centroid Finder algorithm in its FPGA, delivering real-time centroid coordinates at the sensor level. This eliminates round-trip latency and maintains stability under challenging lighting and perspective conditions.

Where the Shape Centroid Finder earns its keep
Precision positioning is central to every inspection and robotic system. In most vision-guided tasks, the controller doesn’t need a full image. It only needs the object’s precise location. The Shape Centroid Algorithm converts complex visual data into deterministic, sub-pixel, low-latency coordinates that remain stable under real-world distortions, providing the most actionable input for any vision-based control system.
Solving engineering challenges in a production-grade centroid
Running a shape centroid finder on an industrial PC is easy for demonstrations but difficult to achieve production-grade reliability. Embedding the algorithm inside the camera’s FPGA adds real value. It removes noise sensitivity, OS jitter, and data overhead, giving system engineers repeatable sub-pixel results with deterministic timing.

Sub-pixel accuracy and robustness in factory condition
At first glance, the centroid formula looks simple, but in practice, achieving sub-pixel accuracy that is repeatable and robust is difficult because:
Noise and lighting variations distort intensity weights, especially near ROI edges.
Thresholding and segmentation strongly affect which pixels enter the calculation.
Non-Gaussian spots or overlapping blobs, distorts the intensity distribution.
Camera response nonlinearity and 8-bit quantization can shift weighted averages.
To address these issues require careful filtering, adaptive thresholding and local fitting and all these will add compute cost and latency. Hardware-based centroid computation inside the camera executes the same logic every frame, eliminating these variations and ensuring consistent results.
Deterministic timing and simplified integration
PC-based centroid processing suffers from OS jitter, bandwidth limits, and complex synchronization, making real-time alignment and control unreliable.
With the Shape Centroid Finder embedded in the camera’s FPGA, centroid data is computed and timestamped at the source, achieving microsecond-level determinism. Only compact coordinate data, typically (x, y, θ, quality), is transmitted. , reducing host load and ensuring stable, scalable performance.
This hardware-level integration eliminates software dependencies and maintenance overhead, delivering consistent, real-time operation across production environments.
Interested? Discuss your needs with usMany customers don’t realize how much more they can do with the camera itself. Take the Shape Centroid Finder as an example — many users buy industrial cameras just to capture images and depend entirely on external software for centroid calculation. With the Shape Centroid Finder built in, our cameras output ready-to-use coordinates directly, eliminating PC-side processing. By understanding the application in detail, we help customers unlock and maximize the camera’s built-in capability for greater efficiency and value.

Beyond finding the centroid: comprehensive shape feature analysis
In addition to precise centroid coordinates, the same on-camera processing can extract advanced geometric features such as aspect ratio, roundness, area, and perimeter. These parameters provide deeper insight into object shape and quality, enabling inspection tasks like solder ball uniformity, nozzle wear detection, or particle classification.
Once these feature values are generated, the camera can further analyze and count how many objects fall within or outside defined tolerances. With these analytics computed directly in the FPGA, engineers gain instant, actionable shape data without added latency or host processing.
Why partner with Basler
Smart vision at the sensor level – Basler integrates the Shape Centroid Finder directly into the camera’s FPGA, turning each device into a smart, deterministic vision sensor for real-time positioning and control.
Proven industrial reliability – Basler’s camera hardware and firmware are designed for consistent, repeatable performance over years of operation, ensuring stable results and minimal maintenance in production environments.
Partnership beyond hardware – Basler’s technical experts work closely with engineers on optical setup, synchronization, and algorithm tuning, helping customers optimize precision, throughput, and scalability across diverse inspection lines.