Customer Story

Goods Logistics with the TORU Picking Robot and the Basler ace Camera

Customer
Magazino GmbH
Location
Munich
Date
2015

The Basler ace camera is a seeing eye for Magazino's intelligent and flexible picking robot TORU. Combined with a cross laser (sheet-of-light method), it enables the robot to locate, measure and grasp objects on shelves.

Speak with a vision expertContact us
Basler ace camera is the seeing eye for Magazino's intelligent and flexible order picking robot TORU
TORU can pick orders in parallel with humans
TORU receives pick orders via WLAN and travels independently to the relevant storage location
TORU receives the pick orders via WLAN and then moves independently to the respective storage location

Use case

From e-commerce to intralogistics in the automotive industry: individual products are needed in all of these areas nowadays and, more rarely, entire pallets. Until now, humans have almost always had to gather the individual objects from the respective warehouses because robots were unable to do so. The gripping process is considered one of the most challenging tasks in robotics. TORU enables the precise measurement and recognition of objects using the Basler ace camera as well as a secure grip on the individual product.

Solution with Basler ace camera

TORU is a mobile robot that can pick orders in warehouses alongside humans. A merchandise management system sends the picking orders to TORU via WLAN, which then moves independently to the relevant storage location. After successful detection using the sheet-of-light method, TORU picks the object and automatically takes it to the desired destination.

Sheet-of-light method excellent for the precise measurement of books with curved spines
The sheet-of-light method is ideal for precisely measuring books with curved spines

Optimal measurement with the sheet-of-light method

In the sheet-of-light method, a cross laser projects two perpendicular laser lines onto the object to be measured. A 2D camera thatBasler ace acA1920-40gmThe laser scanner picks up the reflected laser beams and measures the object based on the position of the lines in the camera image. This process is optimized for cuboid objects such as parcels or shoe boxes. It can also be used to precisely measure books with curved spines.

The quality of the cameras and the implementation of the pylon software interface is very high. Since every support request is answered in the shortest possible time and with well thought-out solutions, we have found a partner we can rely on in Basler AG.
Marcel Debout
Magazino GmbH

The advantages at a glance

  • Lower computing power: In contrast to 3D cameras, the sheet-of-light method with the 2D camera generates fewer 3D points and therefore requires less computing power. This means that the algorithm behind the sheet-of-light method can also be run on a mini-computer, for example.

  • High flexibility of the picking robot

  • Reduction of process costs possible

  • Enables operating time to be extended: it can work in parallel with humans and be integrated into the warehouse during ongoing operations.

  • Adaptability: Thanks to new concepts and high-quality sensor technology, the robot is able to adapt to new situations and changes in the warehouse.

Products used

Get this solution or a customized machine vision solution from us!

Our experts are happy to advise you on your individual vision project.

Magazino - A Jungheinrich Company

Magazino GmbH develops and builds intelligent robots for precise logistics in Industry 4.0. The Munich-based company has set itself the goal of developing new logistics concepts based on autonomous robots. The special feature: Magazino's robots can react to a changing environment - this is only possible thanks to powerful sensor technology, such as a camera.

How can we help you with your logistics automation?

We'd be happy to advise you on product selection and help you find the right vision solution to improve efficiency and reliability.