The adapter kit consists of an adapter board, two flat flex cables, and a power splitter cable. The adapter board converts the GMSL2 signals from up to four cameras into MIPI CSI-2 data. The flat flex cables connect the adapter board and the NVIDIA Jetson Orin Nano Super Developer Kit. The power Y-cable transfers the power supply from the NVIDIA Jetson Orin Nano Super Developer Kit to the adapter board.
A Camera Enablement Package is available to enable plug-and-play use of Basler ace 2 GMSL cameras with the NVIDIA Jetson Orin Nano Super Developer Kit. It contains the necessary configuration for using the adapter kit, making commissioning easier.