Basler Presents the Latest Vision Solutions at Vietnam Industrial Automation Fiesta

From 8 to 10 November 2023, Basler will present its latest vision portfolios and solutions at Vietnam Industrial Automation Fiesta, the signature event that focuses on industrial and robotics automation.

Attendees can expect to see live vision use cases, upgraded product features as well as new products from our portfolio. Key products include our high-speed CXP-12 portfolio and SWIR camera. There will also be a team of Basler’s vision experts on-site to discuss your individual cases and offer suggestions on your projects.

Date: 8-10 November 2023

Location: Kinh Bac Cultural Center Bac Ninh

Booth Number: C37 (Soda Vision Pte. Ltd.)

‌Contact us

Show Highlights

Making The Invisible Visible

Still retaining the familiar sugar cube format, the Basler ace 2 camera is now available in Short-wave infrared (SWIR). Equipped with Sony IMX990/991 SenSWIR sensors, the Basler ace 2 X visSWIR camera has excellent image quality, and a versatile spectrum that sees both visible and invisible light spectrum with wavelengths from 0.4 µm to 1.7 µm. Catch the SWIR camera in action at this exhibition.

Fast Autofocus Vision Solution

A great fit for high-speed applications when the working distance to target objects constantly changes beyond the depth of field and causes conventional fixed focal machine vision to reach its limit. Basler’s own autofocus vision system combines a liquid lens with a fixed focus lens. As such, the solution is not restricted by depth of field, and this allows it to accurately image target objects at various working distances.

Our Highest Resolution Imaging Ever

The two-channel boost R cameras are now available in 127MP – our highest resolution ever. At 17.0 fps and equipped with the highest pixel count sony sensor, the camera is bound to meet your high resolution application requirements.

We look forward to seeing you at the show!

Get in touch to schedule a meeting with our sales team.