Progetto di innovazione

Digital Twin

Vision System Simulations save time and resources

We work with you to find the optimal solution for your application: using a digital twin, we simulate the use of Basler hardware in your system and plan the ideal machine vision system – without time-consuming test setups. You'll benefit from our expertise and save valuable time and resources.

Plan your project with us now
  • Realistic simulation tool

    Easily identify the requirements and challenges of the application
  • Virtual vision system

    Configure cameras, lenses, and lighting without a physical test setup
  • Quickly select the image processing solution

    Saves time and resources, giving a competitive advantage
  • Based on NVIDIA® Omniverse

    Using real-time ray tracing and physics simulation for digital 1:1 mapping

From the digital twin to the Vision System Simulation

A digital twin is a virtual copy of products, processes, or systems. It reproduces real objects or processes exactly. By simulating your application 1:1 in the digital world, we can arrive at your vision solution faster and in a more targeted manner.

A comparison of the scene in the real world (center top) and the digital world (center bottom)

Connecting the real world with the digital world

In the first step, we build the current state in the simulation in great detail. This 1:1 representation of the real world allows us to precisely examine influencing factors and test different configurations—all without the need for elaborate test setups.

In the Vision System Simulator, you can exchange the camera model or lens in just a few clicks to meet the application requirements.

Adjust the configuration in the simulation

Because all of our products are integrated in the Vision System Simulator, any errors in the system structure are shown directly on the PC. Is the image sharp? Is the resolution of the camera sufficient? The simulation answers all these questions directly.

>
Synthetic image data (left) and visualization of the ground truth data for semantic segmentation (right)

Generating synthetic data

By virtually replicating your applications down to the last detail, you receive synthetic data i.e. images of your application. These artificially generated images, together with the ground truth data, can then be used to train AI models for image processing. Thanks to the photo-realistic imaging, the simulation-to-real gap is small enough to effectively use the generated AI model in the real world.

Application Fields for Vision System Simulation

Since we transfer your application into the virtual world, the application fields are almost limitless. This makes it possible to optimize the image processing solution individually for each application.

Logistics application in the digital twin: digitally planned image processing system makes test setups redundant
For applications in the field of electronics, a Digital Twin can be used to plan the ideal image processing system without the need for physical test setups.

Logistic

An example in logistics is to use the simulation to ensure that packages of different sizes can be measured and the barcodes on these packages can be read reliably.

Electronics

In the electronics industry, for example, various lighting units can be tested in different positions when inspecting PCBs. This ensures a reliable image processing solution even with difficult, reflective surfaces.

What does "innovation project" mean? 


When a project is in the innovation phase, we focus on using our customers' experiences to improve the technology for real-world applications - in this case to see how well the Digital Twin technology performs. 

To do this, we want to understand the specific needs and challenges of your application. Based on your feedback, we can improve and move our project forward.

We look forward to having you join our development project!  

What information do we need?  

  • Your contact details

  • How is your application structured and what is the goal?

  • What challenges do you face where the Basler Digital Twin solution could support you?

  • Feedback of any kind

  • Are you already working with NVIDIA® Omniverse? Then we would also be pleased to hear from you

Innovation Thies Justus Group Picture

Implementing a vision solution with a digital twin

Plan your image processing system with Thies Moeller & Justus Basler