Correzione dei pixel nell'imaging SWIR
Il nostro esclusivo algoritmo Pixel Correction Beyond è stato sviluppato per eliminare gli errori di pixel comunemente riscontrati nelle immagini SWIR industriali. Incorporando il contenuto dell'immagine e regolando in modo flessibile l'intensità della correzione, si ottengono risultati significativamente migliori nelle immagini SWIR.

The main hindrance to precise measurement results: defective pixels
Defective pixels occur in the image sensors of digital industrial cameras due to manufacturing defects, aging image sensors, or environmental influences. As a result, they can impair the perceived image quality and thus the accuracy of measurements and image results.

Defective pixels in camera sensors
In particular, defective pixels occur in connection with long exposure times, high gain settings, or a sensor operating at high temperatures (creating hot pixels). Although their number is small, they appear as completely black or white pixels and therefore offer no usable information.
InGaAs sensors are known for their sensitivity to short-wave infrared light. However, they are also inherently prone to pixel defects, with noise levels escalating as sensor temperatures rise.
One Solution: Dynamic defect pixel correction
High measurement accuracy can only be guaranteed by correcting defective pixels. Static correction detects defective pixels during sensor calibration and saves them. Dynamic correction, on the other hand, works continuously on each image while the application is running and can therefore react to changing conditions to correct newly occurring defective pixels. It recognizes and corrects defective pixels even before they leave the camera as image data by adjusting their values to match surrounding pixels in terms of direction and intensity. Such pixel operations are very computationally intensive and time-critical, which is why our Pixel Correction Beyond algorithm is implemented on the camera FPGA.
A further step: Pixel Correction Beyond for SWIR imaging
For industrial users, the question of whether or not to use a cooled SWIR camera hinges on the required image quality. Basler's solution outperforms previous correction algorithms, delivering image quality that matches TEC-based cameras and thus reduce the system cost significantly.

Advantages of Pixel Correction Beyond in SWIR imaging solution
By incorporating the image content, our approach goes beyond conventional dynamic defect pixel correction, offering:
Flexible adjustment of the correction strength
Better correction of structures at the edges of images while retaining image details
Blinking pixels with variable saturation can also be corrected
Our algorithm ensures a uniform and consistent image—and therefore a significant improvement in SWIR imaging quality. Sensitive corrections to image details can be made by adjusting the correction strength. Implementation on a SWIR camera FPGA ensures images are generated at an optimized processing speed without increasing the CPU load.
ace 2 modelli di telecamere visSWIR
Trova la telecamera giusta per la tua applicazione o utilizza il nostro Vision System Configurator per configurare il tuo sistema.