Ваш браузер устарел. Он имеет уязвимости в безопасности и может не показывать все возможности на этом и других сайтах. Узнайте, как обновить Ваш браузер .

OK
Начните настройку системы машинного зрения

В настоящее время Гид по системам машинного зрения не оптимизирован для мобильных устройств.

Back to questions

When you return to the questions section your product selection will be deleted.

Back to Camera Recommandation

If you select a different camera, you will need to specify the appropriate accessories again. Would you like to continue?

All filled in... almost done!

Please let us know in which application the vision system will be used.

Sort by ...

X


List Price

X

Vision Solution Guide (Beta)

Assemble the right vision system for your application - we will guide you to your solution. Answer a few questions and select the vision components that fit and match your requirements. Try this beta version right now!

We look forward to your feedback so we can further improve the tool to meet your needs.

  • Questions

  • Camera Recommendation

  • Accessory Recommendation

  • Your Solution

Questions about your application

  • Do you need color for your solution?

    {{error}} {{getInvalidFieldMessage(1)}}
  • How big is your field of view in mm?

    error {{error1}} {{getInvalidFieldMessage(21)}}
    error {{error2}} {{getInvalidFieldMessage(22)}}
  • What is your working distance in mm?

    error {{error1}} {{getInvalidFieldMessage(31)}}
    error {{error2}} {{getInvalidFieldMessage(32)}}
  • What is the smallest detail to be detected in your application in µm?

    error
    {{error}} {{getInvalidFieldMessage(4) }}
  • Does the object move?

    {{error}} {{getInvalidFieldMessage(5)}}
  • How many frames per second (fps) do you need at least?

    error
    {{error}} {{getInvalidFieldMessage(6)}}
  • At what speed does the object move in mm/s?

    error
    {{error}} {{getInvalidFieldMessage(7)}}
  • What kind of interface do you need? (optional)

    {{error}}
  • What length of data cable do you need in cm? (optional)

    error
    {{error}} {{getInvalidFieldMessage(9)}}

please fill in the mandatory fields

Color / Mono

Field of View

Working Distance

Details Size / Accuracy

Object Motion

Frames per Second

Object Speed

Interface

Data Cable Length

Select "Color" if the color fidelity or coloration of an object is important. If this is not the case, select "Mono". Monochrome cameras have some advantages. These include a higher sensitivity of the sensor compared to color cameras. In addition, no effort is required to create color information. Furthermore, the image information is immediately available in contrast to a color camera, which needs a certain amount of time to reconstruct the color information for each individual pixel.

Field of view (FoV) is the section of the object that is captured by the camera, i.e. that is imaged onto the sensor by the optics. The size of the object has a direct influence on the required resolution or optics of the camera.

In principle, the larger the object, the further away from the camera it should be if it is to be completely captured by the camera. In Machine Vision, there are great differences in the field of views that are used. They range from very small objects (e.g. printed circuit boards or microscopy) to large objects (e.g. vehicles on motorways).

The working distance is the distance between the object and the lens. In combination with the field of view, the working distance defines the required focal length and resolution of the lens or system.

Pay attention to optical distortion, especially if the lens has a short focal length. The working distance should correspond the field of view. In PCB inspection a small field of view and a small working distance is often useful, in a toll bridge a large field of view and a large working distance.

The detail size describes the minimum characteristics to be detected in your field of view. This information is important to determine the right resolution. Resolution is the ability of a vision system to reproduce certain smallest structures.
Especially for the inspection of very small objects (e.g. passive electrical components or small barcodes) a high resolution and accuracy of the system is required. For reliable error detection, the optical resolution should be twice as high as the minimum error: optical resolution = detail size / 2.

Other applications, e.g. Flat Panel Display Inspection, can also have increased requirements with respect to resolution if small details on a large object are to be captured. Below we show one examples to illustrate what the detail size is.

The movement of objects mainly influences the usable shutter type of the camera. Rolling shutter sensors and cameras equipped with them are less expensive, but still offer very good sensitivity. For moving objects, however, their use is very limited.

The frame rate (frames per second) indicates how many frames per second the camera can capture and transmit. Depending on the selected or possible interface, the required resolution and the selected image data format (8bit to 12bit), the frame rates of cameras range from a few frames per second to well over 1,000 frames per second.

For "flowing" images or streams (e.g. when used in microscopy or in the field of sports analysis), at least 25 frames per second should be achieved, or by now even more frequently 60 frames per second.

In classical factory applications (AOI) the camera is often used triggered and the required frame rate is determined by the cycle time of the machine.

Object speed is the speed by which the detected object moves through the field of view.

For example, in a factory, if you want to analyze objects on a conveyor belt, the object speed is the speed of the conveyor belt.

Rule of thumb: The faster the object moves, the higher the demands on the camera, the light and the entire system setup (trigger behavior, exposure time, etc.)

The interface is the combination of hardware and software used to transmit image data from the camera to the downstream system and control data from the system to the camera.

Different interfaces have different advantages and disadvantages with regard to various characteristics such as throughput/bandwidth, cable length, robustness, price, etc.

For example, GigE is widely used and usually already present in the applications and you can access the widely used RJ45 cables.

With USB 3.0, the simple setup (plug and play) and the higher bandwidth compared to GigE can particularly be emphasized.Interfaces such as CameraLink or CoaXPress require special peripherals on the host side, but in return offer advantages in terms of bandwidth and low CPU load.

Important for the choice of interface is the cable length supported by the interface. Depending on the selected interface, there are clear differences.

With GigE cables, long distances of up to 100 m can be bridged when high-quality cables are used With USB 3.0, cable lengths beyond 8-10 m can often only be realized with optical solutions, but with short distances the cables are robust, inexpensive and widely used.

test image test image test image test image test image test image test image test image test image

Your Answers

  • Do you need color for your solution?

    {{questions.monocolor == 'color' ? 'Yes' : questions.monocolor == 'mono' ? 'No' : 'I\'m not sure / I don\'t know' }}
  • How big is your field of view in mm?

    FOV – horizontal: {{questions.fovX}}
    FOV – vertical: {{questions.fovY}}
  • What is your working distance in mm?

    Working Distance (min): {{questions.distanceMin}}
    Working Distance (max): {{questions.distanceMax}}
  • What is the smallest detail to be detected in your application in µm?

    Detail Size: {{questions.detailSize}}
  • Does the object move?

    {{questions.isMovingObject == 'true' ? 'Yes' : 'No'}}
  • How many frames per second (fps) do you need at least?

    FPS min: {{questions.fpsMin == 'nn' ? 'I\'m not sure / I don\'t know': questions.fpsMin}}
  • At what speed does the object move in mm/s?

    Speed: {{questions.vMax}}
  • What kind of interface do you need? (optional)

    Interface: {{index > 0 ? ', ': ''}}{{mapInterfaceInput(option)}}
  • What length of data cable do you need in cm? (optional)

    Length (min): {{questions.cableLength}}

Camera ({{cameras.length}})

In order to be able to recommend further vision components, please select a camera first.

Sorry, we couldn’t find a camera matching your requirements.

Please have a look at the following questions again and adjust your entries if possible.

  • How big is your field of view in mm?
  • What is your detail size / accuracy in µm?
  • Does the object move?

If you still get no result, then contact our support - we are happy to help you.

camera
{{camera.cameraSeries}} - {{camera.modelName}}
Resolution (HxV) (px)
{{camera.resolutionHVDisplay}}
Resolution (MP)
{{camera.resolutionDisplay}}
Sensor
{{camera.sensorNameDisplay}}
Sensorsize
{{camera.sensorSizeDisplay}}
Pixelsize
{{camera.pixelSizeDisplay}}
Frame Rate (fps)
{{camera.framerateDisplay}}
Mono/Color
{{camera.monocolorDisplay}}
Interface
{{camera.interfaceDisplay}}
Housing Size
{{camera.housingsizeDisplay}}
Details

Camera ({{cameras.length}})

camera
{{selectedCamera.cameraSeries}} - {{selectedCamera.modelName}}
Resolution (HxV) (px)
{{selectedCamera.resolutionHVDisplay}}
Resolution (MP)
{{selectedCamera.resolutionDisplay}}
Sensor
{{selectedCamera.sensorNameDisplay}}
Sensorsize
{{selectedCamera.sensorSizeDisplay}}
Pixelsize
{{selectedCamera.pixelSizeDisplay}}
Frame Rate (fps)
{{selectedCamera.framerateDisplay}}
Mono/Color
{{selectedCamera.monocolorDisplay}}
Interface
{{selectedCamera.interfaceDisplay}}
Housing Size
{{selectedCamera.housingsizeDisplay}}

Lens ({{objectives.length}})

camera
{{selectedObjective.modelName}}
Lens Mount
{{selectedObjective.lensMountDisplay}}
Sensor Format
{{selectedObjective.maxImageCircleDisplay}}
Focal Length
{{selectedObjective.focalLengthDisplay}}
Iris Range
{{selectedObjective.irisDisplay}}
Required Working Distance
This is a precise approximate value that applies from the front edge of the lens. The lens may have tolerances - this should be verified in a test setup.
{{selectedObjective.distance}} mm

Sorry, we couldn’t find a match for your requirements.

Please check your entries again or contact our support department - we are happy to help you.

camera
{{objective.modelName}}
Lens Mount
{{objective.lensMountDisplay}}
Sensor Format
{{objective.maxImageCircleDisplay}}
Focal Length
{{objective.focalLengthDisplay}}
Iris Range
{{objective.irisDisplay}}
Required Working Distance
This is a precise approximate value that applies from the front edge of the lens. The lens may have tolerances - this should be verified in a test setup.
{{objective.distance}} mm
Details

Power Cable ({{powercables.length}})

camera
{{selectedPowercable.modelName}}
Interface
{{selectedPowercable.interfaceDisplay}}
Connector Camera Side
{{selectedPowercable.connectorCameraSideDisplay}}
Accessory Type
{{selectedPowercable.accessoryTypeDisplay}}

Sorry, we couldn’t find a match for your requirements.

Please check your entries again or contact our support department - we are happy to help you.

camera
{{powercable.modelName}}
Interface
{{powercable.interfaceDisplay}}
Connector Camera Side
{{powercable.connectorCameraSideDisplay}}
Accessory Type
{{powercable.accessoryTypeDisplay}}
Details

Data Cable ({{datacables.length}})

camera
{{selectedDatacable.modelName}}
Interface
{{selectedDatacable.interfaceDisplay}}
Connector Camera Side
{{selectedDatacable.connectorCameraSideDisplay}}
Connector Host
{{selectedDatacable.connectorHostSideDisplay}}
Accessory Type
{{selectedDatacable.accessoryTypeDisplay}}
Length (min)
{{selectedDatacable.cableLengthDisplay}}

Sorry, we couldn’t find a match for your requirements.

Please check your entries again or contact our support department - we are happy to help you.

camera
{{datacable.modelName}}
Interface
{{datacable.interfaceDisplay}}
Connector Camera Side
{{datacable.connectorCameraSideDisplay}}
Connector Host
{{datacable.connectorHostSideDisplay}}
Accessory Type
{{datacable.accessoryTypeDisplay}}
Length (min)
{{datacable.cableLengthDisplay}}
Details

Interface Card ({{pccards.length}})

camera
{{selectedPcCard.modelName}}
Interface
{{selectedPcCard.interfaceDisplay}}
Number of Ports
{{selectedPcCard.noofportsDisplay}}

Sorry, we couldn’t find a match for your requirements.

Please check your entries again or contact our support department - we are happy to help you.

camera
{{pccard.modelName}}
Interface
{{pccard.interfaceDisplay}}
Number of Ports
{{pccard.noofportsDisplay}}
Details

Your Solution

camera
{{selectedCamera.cameraSeries}} - {{selectedCamera.modelName}}
Resolution (HxV) (px)
{{selectedCamera.resolutionHVDisplay}}
Resolution (MP)
{{selectedCamera.resolutionDisplay}}
Sensor
{{selectedCamera.sensorNameDisplay}}
Sensorsize
{{selectedCamera.sensorSizeDisplay}}
Pixelsize
{{selectedCamera.pixelSizeDisplay}}
Frame Rate (fps)
{{selectedCamera.framerateDisplay}}
Mono/Color
{{selectedCamera.monocolorDisplay}}
Interface
{{selectedCamera.interfaceDisplay}}
Housing Size
{{selectedCamera.housingsizeDisplay}}
Objective
{{selectedObjective.modelName}}
Lens Mount
{{selectedObjective.lensMountDisplay}}
Sensor Format
{{selectedObjective.maxImageCircleDisplay}}
Focal Length
{{selectedObjective.focalLengthDisplay}}
Iris Range
{{selectedObjective.irisDisplay}}
Required Working Distance
This is a precise approximate value that applies from the front edge of the lens. The lens may have tolerances - this should be verified in a test setup.
{{selectedObjective.distance}} mm
Powercable
{{selectedPowercable.modelName}}
Interface
{{selectedPowercable.interfaceDisplay}}
Connector Camera Side
{{selectedPowercable.connectorCameraSideDisplay}}
Accessory Type
{{selectedPowercable.accessoryTypeDisplay}}
Datacable
{{selectedDatacable.modelName}}
Interface
{{selectedDatacable.interfaceDisplay}}
Connector Camera Side
{{selectedDatacable.connectorCameraSideDisplay}}
Connector Host
{{selectedDatacable.connectorHostSideDisplay}}
Accessory Type
{{selectedDatacable.accessoryTypeDisplay}}
Length (min)
{{selectedDatacable.cableLengthDisplay}}
pcCard
{{selectedPcCard.modelName}}
Interface
{{selectedPcCard.interfaceDisplay}}
Number of Ports
{{selectedPcCard.noofportsDisplay}}

Total Sum

{{gui.summaryArticle}} component(s)

For pricing, please use the request cart to get a quote.

Buy now in Shop