Your browser is out of date. It may not display all features of this websites. Learn how to update your browser.

OK
Careers | Investors

Success Stories

In Line with the Printing Industry: Label Inspection with Basler sprint Camera Link Cameras

A B Graphic International Ltd is a leading company within the label printing industry. It also produces machines for many specialist applications including RFID insertion, laser die cutting, booklet label insertion machines and 100 % camera inspection systems for labels, foils, blisters, sheets and package boxes.

In the printing industry, speed is generally a decisive factor. A reliable printing inspection must be able to detect quite a number of different print errors such as scratches, text irregularities, ink blobs, registration shifts and even color variations. It must be able to read codified information, as barcode or OCR code, or to meter distances between significant points of the label, too, when the customer requires it. Therefore not only speed, but also resolution and color fidelity were important requirements for the cameras to be used in the inspection system. The system setup must be capable of working with different label support materials, like paper, reflecting plastic and metal foils, and even holograms. A B Graphic International chose Basler sprint cameras to achieve the required high speed, high resolution and excellent image quality.

Download now for free

Please select a language version to start your download.