Your browser is out of date. It may not display all features of this websites. Learn how to update your browser.

OK
Careers | Investors

Application Notes

Interfacing Basler cameras with the Matrox MIL software

Document number: AW000648

The document describes the requirements and necessary adjustments for using a Basler GigE or USB 3.0 Vision camera with the Matrox Imaging Library (MIL) software. The following issues are covered:

  • Hardware requirements for using a Basler GigE Vision or USB 3.0 Vision camera.
  • Installation of the Matrox Imaging Library 10
  • If a Basler GigE Vision camera is used:
  • Setting up the MIL Config application for camera detection.
  • Configuring the IP address for the GigE network adapter using the Matrox Capture Assistant.
  • Configuring the camera’s IP address and adjusting transport layer parameters to maximize bandwidth.
  • If a Basler USB 3.0 Vision camera is used:
  • Installing the Matrox USB3 Vision Driver
  • Accessing the camera using the Matrox Intellicam software and adjusting, if necessary, settings for the driver or license.
  • Troubleshooting for GigE cameras, addressing the network adapter’s firewall and transport layer settings.

Download now for free

Please click on the following link to start your download.