Your browser is out of date. It may not display all features of this websites. Learn how to update your browser.

OK
Careers | Investors

Brochures

Accuracy of Basler ToF Camera - Brochure

This document contains measurements related to the precision of the Basler ToF camera, as well as the conditions under which those values were gathered.
The precision of the Basler ToF camera was tested under the following lab conditions:

  • Ambient temperature: 22 °C
  • 20 minutes of warm-up time for the camera
  • 25 test images
  • No ambient light

To determine the precision level, the difference between the measured distance and the actual distance was calculated. This brochure goes into more detail on the procedure.

Download now for free

Please click on the following link to start your download.