Your browser is out of date. It may not display all features of this websites. Learn how to update your browser.

OK
Careers | Investors
  • CCD’s been discontinued. Now what?

    Experience together with Steve what Sony’s CCD discontinuation announcement means and how you can deal with it.

    Just press play!

Switching from CCD to CMOS Cameras

Switching from CCD to CMOS Cameras

Sony has stopped the production of CCD sensors. CCD camera users are now confronted with questions around switching to CMOS technology and the availability of current CCD camera models.

For us, the move toward CMOS technology doesn’t come as a surprise. We started our preparations some time ago and can offer a broad portfolio of CMOS products.

Basler will ensure a smooth transition from current Basler products with CCD sensors to CMOS sensor-based Basler products.

We’ve put together a list of answers to the most relevant questions around this transition and around suitable successors for your CCD sensor-based ace camera.

Below you can find answers for the most frequently asked questions about this topic:

When should I begin switching from CCD to CMOS?

In general, you could start any time. Switching quickly will let you benefit from a performance increase in your application and from lower camera costs. Therefore, a fast change makes sense, especially since we have already discontinued the first CCD camera models due to the unexpectedly high demand. An overview of all discontinued models can be found here. We recommend taking the time to run the calculations on your application, to decide which option would be more advantageous.

What do I have to consider when switching?

Relatively little. You shouldn’t have any trouble finding a camera with a suitable CMOS sensor. For an easy switch, choose a CMOS sensor with the same optical format as your current CCD cameras, and you’ll only have to perform minimal adjustments to your system design. Things are also kept simple if you stay with your standard interface, Gigabit Ethernet. Basler offers all new CMOS sensors within the 29 mm x 29 mm housing of its ace models which allows for easy replacement of nearly all existing camera designs. It also brings along improved performance in replacement scenarios of analog FireWire cameras, where space limits are a crucial concern.

What’s important when integrating the latest CMOS-based cameras?

Integrating a CMOS camera to replace CCD sensors is simpler than expected, especially when you choose standard-compliant hardware and software. Because camera manufacturers take care of the entire sensor integration including image quality optimization, all you need to do when choosing the right CMOS camera is to:

  • Determine the correct resolution of the camera: The required resolution depends on the details you need to make visible in your images.
  • Define the required camera interface: The choice of an interface depends on the required cable length, bandwidth, necessary frame rates and real-time capabilities and PC hardware availability. Our Interface Advisor helps you find the best interface for your application.
  • Choose lens and lighting: Changing the sensor format also involves changing the lens. Our Lens Selector makes finding a new lens easy. Lighting must only be adjusted if the sensitivity of the new sensor is different from the previous one.
  • Integration effort for software and camera control: Cameras complying with common standards such as GenICam, for example, or interface standards like USB3 Vision or GigE Vision, offer uncomplicated integration.

Which CMOS Replacements are Already Available from Basler?

Basler has anticipated the trend towards CMOS sensor technology in industrial cameras early on and offers a broad product portfolio of CMOS cameras with sensors from various manufacturers. Just recently, it equipped two ace GigE and two ace USB 3.0 models with Sony’s IMX174 CMOS sensor. With a resolution of 2.3 MP and frame rates of 50 fps (GigE) and 155 fps (USB 3.0), respectively, this powerful sensor is a recommended choice for demanding applications in the fields of traffic, microscopy and medicine.

Furthermore, several ace models were equipped with CMOS sensors of the PYTHON series from ON Semiconductor. These models reach speeds of up to 850 fps and impress with their outstanding image quality.

A comprehensive overview of all CMOS successors for the various Basler CCD cameras is available right here.

Overview of potential successor cameras

Are you using a CCD camera and looking for the right replacement with CMOS technology? With the help of our CCD Transition Advisor, you can get an overview of all suitable replacement models for your CCD camera with just a few clicks.

Reset filters

The following CMOS sensors are well suited to replace your CCD sensor:

IMX174

IMX174
  • Pixel Size: 5,86 µm x 5,86 µm
  • Max. Image Circle: 1/1.2"
  • Resolution: 1920 px x 1200 px

IMX252

IMX252
  • Pixel Size: 3,45 µm x 3,45 µm
  • Max. Image Circle: 1/1.8"
  • Resolution: 2048 px x 1536 px

IMX273

IMX273
  • Pixel Size: 3,45 µm x 3,45 µm
  • Max. Image Circle: 1/2.9"
  • Resolution: 1440 px x 1080 px

IMX178

IMX178
  • Pixel Size: 2,4 µm x 2,4 µm
  • Max. Image Circle: 1/1.8"
  • Resolution: 3088 px x 2064 px

IMX174

IMX174
  • Pixel Size: 5,86 µm x 5,86 µm
  • Max. Image Circle: 1/1.2"
  • Resolution: 1920 px x 1200 px

IMX252

IMX252
  • Pixel Size: 3,45 µm x 3,45 µm
  • Max. Image Circle: 1/1.8"
  • Resolution: 2048 px x 1536 px

PYTHON 2000

PYTHON 2000
  • Pixel Size: 4,8 µm x 4,8 µm
  • Max. Image Circle: 2/3"
  • Resolution: 1920 px x 1200 px

IMX178

IMX178
  • Pixel Size: 2,4 µm x 2,4 µm
  • Max. Image Circle: 1/1.8"
  • Resolution: 3088 px x 2064 px

IMX174

IMX174
  • Pixel Size: 5,86 µm x 5,86 µm
  • Max. Image Circle: 1/1.2"
  • Resolution: 1920 px x 1200 px

IMX252

IMX252
  • Pixel Size: 3,45 µm x 3,45 µm
  • Max. Image Circle: 1/1.8"
  • Resolution: 2048 px x 1536 px

PYTHON 1300

PYTHON 1300
  • Pixel Size: 4,8 µm x 4,8 µm
  • Max. Image Circle: 1/2"
  • Resolution: 1280 px x 1024 px

IMX273

IMX273
  • Pixel Size: 3,45 µm x 3,45 µm
  • Max. Image Circle: 1/2.9"
  • Resolution: 1440 px x 1080 px

IMX178

IMX178
  • Pixel Size: 2,4 µm x 2,4 µm
  • Max. Image Circle: 1/1.8"
  • Resolution: 3088 px x 2064 px

IMX265

IMX265
  • Pixel Size: 3,45 µm x 3,45 µm
  • Max. Image Circle: 1/1.8"
  • Resolution: 2048 px x 1536 px

IMX249

IMX249
  • Pixel Size: 5,86 µm x 5,86 µm
  • Max. Image Circle: 1/1.2"
  • Resolution: 1920 px x 1200 px

EV76C570

EV76C570
  • Pixel Size: 4,5 µm x 4,5 µm
  • Max. Image Circle: 1/1.8"
  • Resolution: 1600 px x 1200 px

IMX178

IMX178
  • Pixel Size: 2,4 µm x 2,4 µm
  • Max. Image Circle: 1/1.8"
  • Resolution: 3088 px x 2064 px

IMX174

IMX174
  • Pixel Size: 5,86 µm x 5,86 µm
  • Max. Image Circle: 1/1.2"
  • Resolution: 1920 px x 1200 px

IMX250

IMX250
  • Pixel Size: 3,45 µm x 3,45 µm
  • Max. Image Circle: 2/3"
  • Resolution: 2448 px x 2048 px

IMX264

IMX264
  • Pixel Size: 3,45 µm x 3,45 µm
  • Max. Image Circle: 2/3"
  • Resolution: 2448 px x 2048 px

IMX249

IMX249
  • Pixel Size: 5,86 µm x 5,86 µm
  • Max. Image Circle: 1/1.2"
  • Resolution: 1920 px x 1200 px

IMX287

IMX287
  • Pixel Size: 6,9 µm x 6,9 µm
  • Max. Image Circle: 1/2.9"
  • Resolution: 720 px x 540 px

IMX265

IMX265
  • Pixel Size: 3,45 µm x 3,45 µm
  • Max. Image Circle: 1/1.8"
  • Resolution: 2048 px x 1536 px

IMX249

IMX249
  • Pixel Size: 5,86 µm x 5,86 µm
  • Max. Image Circle: 1/1.2"
  • Resolution: 1920 px x 1200 px

PYTHON 1300

PYTHON 1300
  • Pixel Size: 4,8 µm x 4,8 µm
  • Max. Image Circle: 1/2"
  • Resolution: 1280 px x 1024 px

IMX287

IMX287
  • Pixel Size: 6,9 µm x 6,9 µm
  • Max. Image Circle: 1/2.9"
  • Resolution: 720 px x 540 px

IMX249

IMX249
  • Pixel Size: 5,86 µm x 5,86 µm
  • Max. Image Circle: 1/1.2"
  • Resolution: 1920 px x 1200 px

PYTHON 1300

PYTHON 1300
  • Pixel Size: 4,8 µm x 4,8 µm
  • Max. Image Circle: 1/2"
  • Resolution: 1280 px x 1024 px

IMX265

IMX265
  • Pixel Size: 3,45 µm x 3,45 µm
  • Max. Image Circle: 1/1.8"
  • Resolution: 2048 px x 1536 px

PYTHON 2000

PYTHON 2000
  • Pixel Size: 4,8 µm x 4,8 µm
  • Max. Image Circle: 2/3"
  • Resolution: 1920 px x 1200 px

IMX287

IMX287
  • Pixel Size: 6,9 µm x 6,9 µm
  • Max. Image Circle: 1/2.9"
  • Resolution: 720 px x 540 px

IMX249

IMX249
  • Pixel Size: 5,86 µm x 5,86 µm
  • Max. Image Circle: 1/1.2"
  • Resolution: 1920 px x 1200 px

PYTHON 1300

PYTHON 1300
  • Pixel Size: 4,8 µm x 4,8 µm
  • Max. Image Circle: 1/2"
  • Resolution: 1280 px x 1024 px

IMX273

IMX273
  • Pixel Size: 3,45 µm x 3,45 µm
  • Max. Image Circle: 1/2.9"
  • Resolution: 1440 px x 1080 px

IMX249

IMX249
  • Pixel Size: 5,86 µm x 5,86 µm
  • Max. Image Circle: 1/1.2"
  • Resolution: 1920 px x 1200 px

IMX265

IMX265
  • Pixel Size: 3,45 µm x 3,45 µm
  • Max. Image Circle: 1/1.8"
  • Resolution: 2048 px x 1536 px

EV76C560

EV76C560
  • Pixel Size: 5,3 µm x 5,3 µm
  • Max. Image Circle: 1/1.8"
  • Resolution: 1280 px x 1024 px

ICX618 Replacement

ICX618 Replacement
  • Pixel Size: 5,6 µm x 5,6 µm
  • Max. Image Circle: 1/4"
  • Resolution: 659 px x 494 px

PYTHON 300

PYTHON 300
  • Pixel Size: 4,8 µm x 4,8 µm
  • Max. Image Circle: 1/4"
  • Resolution: 640 px x 480 px

IMX249

IMX249
  • Pixel Size: 5,86 µm x 5,86 µm
  • Max. Image Circle: 1/1.2"
  • Resolution: 1920 px x 1200 px

IMX287

IMX287
  • Pixel Size: 6,9 µm x 6,9 µm
  • Max. Image Circle: 1/2.9"
  • Resolution: 720 px x 540 px

IMX250

IMX250
  • Pixel Size: 3,45 µm x 3,45 µm
  • Max. Image Circle: 2/3"
  • Resolution: 2448 px x 2048 px

IMX264

IMX264
  • Pixel Size: 3,45 µm x 3,45 µm
  • Max. Image Circle: 2/3"
  • Resolution: 2448 px x 2048 px

PYTHON 5000

PYTHON 5000
  • Pixel Size: 4,8 µm x 4,8 µm
  • Max. Image Circle: 1"
  • Resolution: 2590 px x 2048 px

IMX250

IMX250
  • Pixel Size: 3,45 µm x 3,45 µm
  • Max. Image Circle: 2/3"
  • Resolution: 2448 px x 2048 px

IMX264

IMX264
  • Pixel Size: 3,45 µm x 3,45 µm
  • Max. Image Circle: 2/3"
  • Resolution: 2448 px x 2048 px

IMX252

IMX252
  • Pixel Size: 3,45 µm x 3,45 µm
  • Max. Image Circle: 1/1.8"
  • Resolution: 2048 px x 1536 px

PYTHON 5000

PYTHON 5000
  • Pixel Size: 4,8 µm x 4,8 µm
  • Max. Image Circle: 1"
  • Resolution: 2590 px x 2048 px

IMX267

IMX267
  • Pixel Size: 3,45 µm x 3,45 µm
  • Max. Image Circle: 1"
  • Resolution: 4096 px x 2160 px

IMX255

IMX255
  • Pixel Size: 3,45 µm x 3,45 µm
  • Max. Image Circle: 1"
  • Resolution: 4096 px x 2168 px

IMX267

IMX267
  • Pixel Size: 3,45 µm x 3,45 µm
  • Max. Image Circle: 1"
  • Resolution: 4096 px x 2160 px

IMX253

IMX253
  • Pixel Size: 3,45 µm x 3,45 µm
  • Max. Image Circle: 1.1"
  • Resolution: 4096 px x 3000 px

IMX304

IMX304
  • Pixel Size: 3,45 µm x 3,45 µm
  • Max. Image Circle: 1.1"
  • Resolution: 4096 px x 3000 px

IMX253

IMX253
  • Pixel Size: 3,45 µm x 3,45 µm
  • Max. Image Circle: 1.1"
  • Resolution: 4096 px x 3000 px

IMX304

IMX304
  • Pixel Size: 3,45 µm x 3,45 µm
  • Max. Image Circle: 1.1"
  • Resolution: 4096 px x 3000 px
Please choose your CCD sensor.

There are 195 elements available for filtering.

Your choice of Basler CMOS cameras:  0

Camera model Interface Mono/Color Availability i
100000 AR0134
daA1280-54lc (S-Mount) BCON for LVDS Color AR0134
100001 AR0134
daA1280-54lm (S-Mount) BCON for LVDS Mono AR0134
100002 AR0134
daA1280-54uc (No-Mount) USB 3.0 Color AR0134
100003 AR0134
daA1280-54um (No-Mount) USB 3.0 Mono AR0134
100004 AR0134
daA1280-54um (S-Mount) USB 3.0 Mono AR0134
100005 AR0134
daA1280-54um (CS-Mount) USB 3.0 Mono AR0134
100006 AR0134
daA1280-54uc (CS-Mount) USB 3.0 Color AR0134
100007 AR0134
daA1280-54uc (S-Mount) USB 3.0 Color AR0134
100008 AR0134
daA1280-54lm (No-Mount) BCON for LVDS Mono AR0134
100009 AR0134
daA1280-54lm (CS-Mount) BCON for LVDS Mono AR0134
100010 AR0134
daA1280-54lc (No-Mount) BCON for LVDS Color AR0134
100011 AR0134
daA1280-54lc (CS-Mount) BCON for LVDS Color AR0134
100012 AR0134
puA1280-54uc USB 3.0 Color AR0134
100013 AR0134
puA1280-54um USB 3.0 Mono AR0134
100014 AR0521
daA2500-60mc (S-Mount) BCON for MIPI Color AR0521 Series Production: now
100015 AR0521
daA2500-60mc (No-Mount) BCON for MIPI Color AR0521 Series Production: now
100016 AR0521
daA2500-60mc (No-Mount) - Tray (40pcs) BCON for MIPI Color AR0521 Series Production: now
100017 AR0521
daA2500-60mc (S-Mount) – Tray (40pcs) BCON for MIPI Color AR0521 Series Production: now
100018 CMV12000
beA4000-62kc Camera Link Color CMV12000
100019 CMV12000
beA4000-62km Camera Link Mono CMV12000
100020 CMV2000
acA2000-165uc USB 3.0 Color CMV2000
100021 CMV2000
acA2000-165um USB 3.0 Mono CMV2000
100022 CMV2000
acA2000-340kc Camera Link Color CMV2000
100023 CMV2000
acA2000-340km Camera Link Mono CMV2000
100024 CMV2000
acA2000-50gc GigE Color CMV2000
100025 CMV2000
acA2000-50gm GigE Mono CMV2000
100026 CMV2000 NIR-enhanced
acA2000-165umNIR USB 3.0 Mono CMV2000 NIR-enhanced
100027 CMV2000 NIR-enhanced
acA2000-340kmNIR Camera Link Mono CMV2000 NIR-enhanced
100028 CMV2000 NIR-enhanced
acA2000-50gmNIR GigE Mono CMV2000 NIR-enhanced
100029 CMV4000
acA2040-180kc Camera Link Color CMV4000
100030 CMV4000
acA2040-180km Camera Link Mono CMV4000
100031 CMV4000
acA2040-25gc GigE Color CMV4000
100032 CMV4000
acA2040-25gm GigE Mono CMV4000
100033 CMV4000
acA2040-90uc USB 3.0 Color CMV4000
100034 CMV4000
acA2040-90um USB 3.0 Mono CMV4000
100035 CMV4000 NIR-enhanced
acA2040-180kmNIR Camera Link Mono CMV4000 NIR-enhanced
100036 CMV4000 NIR-enhanced
acA2040-25gmNIR GigE Mono CMV4000 NIR-enhanced
100037 CMV4000 NIR-enhanced
acA2040-90umNIR USB 3.0 Mono CMV4000 NIR-enhanced
100038 EV76C560
acA1280-60gc GigE Color EV76C560
100039 EV76C560
acA1280-60gm GigE Mono EV76C560
100040 EV76C560
acA1300-60gc GigE Color EV76C560
100041 EV76C560
acA1300-60gm GigE Mono EV76C560
100042 EV76C570
acA1600-60gc GigE Color EV76C570
100043 EV76C570
acA1600-60gm GigE Mono EV76C570
100044 EV76C570
daA1600-60uc (No-Mount) USB 3.0 Color EV76C570
100045 EV76C570
daA1600-60um (CS-Mount) USB 3.0 Mono EV76C570
100046 EV76C570
daA1600-60lc (S-Mount) BCON for LVDS Color EV76C570
100047 EV76C570
daA1600-60lm (S-Mount) BCON for LVDS Mono EV76C570
100048 EV76C570
daA1600-60um (No-Mount) USB 3.0 Mono EV76C570
100049 EV76C570
daA1600-60um (S-Mount) USB 3.0 Mono EV76C570
100050 EV76C570
daA1600-60uc (CS-Mount) USB 3.0 Color EV76C570
100051 EV76C570
daA1600-60uc (S-Mount) USB 3.0 Color EV76C570
100052 EV76C570
daA1600-60lm (No-Mount) BCON for LVDS Mono EV76C570
100053 EV76C570
daA1600-60lm (CS-Mount) BCON for LVDS Mono EV76C570
100054 EV76C570
daA1600-60lc (No-Mount) BCON for LVDS Color EV76C570
100055 EV76C570
daA1600-60lc (CS-Mount) BCON for LVDS Color EV76C570
100056 EV76C570
puA1600-60uc USB 3.0 Color EV76C570
100057 EV76C570
puA1600-60um USB 3.0 Mono EV76C570
100058 EV76C661
acA1300-60gmNIR GigE Mono EV76C661
100059 ICX618 Replacement
acA640-121gm GigE Mono ICX618 Replacement Design-In Sample: now
Series Production: now
100060 IMX174
acA1920-155uc USB 3.0 Color IMX174
100061 IMX174
acA1920-155um USB 3.0 Mono IMX174
100062 IMX174
acA1920-50gc GigE Color IMX174
100063 IMX174
acA1920-50gm GigE Mono IMX174
100064 IMX174
Basler MED ace 2.3 MP 164 color USB 3.0 Color IMX174 Series Production: now
100065 IMX174
Basler MED ace 2.3 MP 164 mono USB 3.0 Mono IMX174 Series Production: now
100066 IMX178
acA3088-57um USB 3.0 Mono IMX178
100067 IMX178
acA3088-57uc USB 3.0 Color IMX178
100068 IMX178
acA3088-16gm GigE Mono IMX178
100069 IMX178
acA3088-16gc GigE Color IMX178
100070 IMX183
acA5472-17um USB 3.0 Mono IMX183 Series Production: now
100071 IMX183
acA5472-17uc USB 3.0 Color IMX183 Series Production: now
100072 IMX183
acA5472-5gm GigE Mono IMX183 Series Production: now
100073 IMX183
acA5472-5gc GigE Color IMX183 Series Production: now
100074 IMX183
Basler MED ace 20.0 MP 17 mono USB 3.0 Mono IMX183 Series Production: tbd
100075 IMX183
Basler MED ace 20.0 MP 17 color USB 3.0 Color IMX183 Series Production: tbd
100076 IMX226
acA4024-29um USB 3.0 Mono IMX226
100077 IMX226
acA4024-29uc USB 3.0 Color IMX226
100078 IMX226
acA4024-8gm GigE Mono IMX226
100079 IMX226
acA4024-8gc GigE Color IMX226
100080 IMX249
acA1920-40gc GigE Color IMX249
100081 IMX249
acA1920-40gm GigE Mono IMX249
100082 IMX249
acA1920-40uc USB 3.0 Color IMX249
100083 IMX249
acA1920-40um USB 3.0 Mono IMX249
100084 IMX249
Basler MED ace 2.3 MP 41 color USB 3.0 Color IMX249 Series Production: now
100085 IMX249
Basler MED ace 2.3 MP 41 mono USB 3.0 Mono IMX249 Series Production: now
100086 IMX250
acA2440-75uc USB 3.0 Color IMX250
100087 IMX250
acA2440-75um USB 3.0 Mono IMX250
100088 IMX250
Basler MED ace 5.1 MP 75 color USB 3.0 Color IMX250 Series Production: now
100089 IMX250
Basler MED ace 5.1 MP 75 mono USB 3.0 Mono IMX250 Series Production: now
100090 IMX252
acA2040-120uc USB 3.0 Color IMX252
100091 IMX252
acA2040-120um USB 3.0 Mono IMX252
100092 IMX253
acA4112-30um USB 3.0 Mono IMX253
100093 IMX253
acA4112-30uc USB 3.0 Color IMX253
100094 IMX253
boA4112-68cm CoaXPress Mono IMX253 Design-In Sample: Q3/2019
Series Production: Q4/2019
100095 IMX253
boA4112-68cc CoaXPress Color IMX253 Design-In Sample: Q3/2019
Series Production: Q4/2019
100096 IMX253
Basler MED ace 12.3 MP 30 color USB 3.0 Color IMX253 Design-In Sample: April 2019
Series Production: Q2/2019
100097 IMX253
Basler MED ace 12.3 MP 30 mono USB 3.0 Mono IMX253 Design-In Sample: April 2019
Series Production: Q2/2019
100098 IMX255
acA4096-40um USB 3.0 Mono IMX255
100099 IMX255
acA4096-40uc USB 3.0 Color IMX255
100100 IMX255
boA4096-93cc CoaXPress Color IMX255 Design-In Sample: Q3/2019
Series Production: Q4/2019
100101 IMX255
boA4096-93cm CoaXPress Mono IMX255 Design-In Sample: Q3/2019
Series Production: Q4/2019
100102 IMX255
Basler MED ace 8.9 MP 42 color USB 3.0 Color IMX255 Design-In Sample: April 2019
Series Production: Q2/2019
100103 IMX255
Basler MED ace 8.9 MP 42 mono USB 3.0 Mono IMX255 Design-In Sample: April 2019
Series Production: Q2/2019
100104 IMX264
acA2440-20gc GigE Color IMX264
100105 IMX264
acA2440-20gm GigE Mono IMX264
100106 IMX264
acA2440-35uc USB 3.0 Color IMX264
100107 IMX264
acA2440-35um USB 3.0 Mono IMX264
100108 IMX264
Basler MED ace 5.1 MP 35 color USB 3.0 Color IMX264 Series Production: now
100109 IMX264
Basler MED ace 5.1 MP 35 mono USB 3.0 Mono IMX264 Series Production: now
100110 IMX265
acA2040-35gc GigE Color IMX265
100111 IMX265
acA2040-35gm GigE Mono IMX265
100112 IMX265
acA2040-55uc USB 3.0 Color IMX265
100113 IMX265
acA2040-55um USB 3.0 Mono IMX265
100114 IMX267
acA4096-30um USB 3.0 Mono IMX267
100115 IMX267
acA4096-30uc USB 3.0 Color IMX267
100116 IMX267
acA4096-11gm GigE Mono IMX267
100117 IMX267
acA4096-11gc GigE Color IMX267
100118 IMX267
Basler MED ace 8.9 MP 32 color USB 3.0 Color IMX267 Design-In Sample: April 2019
Series Production: Q2/2019
100119 IMX267
Basler MED ace 8.9 MP 32 mono USB 3.0 Mono IMX267 Design-In Sample: April 2019
Series Production: Q2/2019
100120 IMX273
acA1440-73gm GigE Mono IMX273
100121 IMX273
acA1440-73gc GigE Color IMX273
100122 IMX273
acA1440-220uc USB 3.0 Color IMX273
100123 IMX273
acA1440-220um USB 3.0 Mono IMX273
100124 IMX287
acA720-290gm GigE Mono IMX287
100125 IMX287
acA720-290gc GigE Color IMX287
100126 IMX287
acA720-520uc USB 3.0 Color IMX287
100127 IMX287
acA720-520um USB 3.0 Mono IMX287
100128 IMX304
acA4112-20um USB 3.0 Mono IMX304
100129 IMX304
acA4112-20uc USB 3.0 Color IMX304
100130 IMX304
acA4112-8gm GigE Mono IMX304
100131 IMX304
acA4112-8gc GigE Color IMX304
100132 IMX304
Basler MED ace 12.3 MP 23 color USB 3.0 Color IMX304 Design-In Sample: April 2019
Series Production: Q2/2019
100133 IMX304
Basler MED ace 12.3 MP 23 mono USB 3.0 Mono IMX304 Design-In Sample: April 2019
Series Production: Q2/2019
100134 MT9F002
acA4600-10uc USB 3.0 Color MT9F002
100135 MT9F002
acA4600-7gc GigE Color MT9F002
100136 MT9J003
acA3800-10gc GigE Color MT9J003
100137 MT9J003
acA3800-10gm GigE Mono MT9J003
100138 MT9J003
acA3800-14uc USB 3.0 Color MT9J003
100139 MT9J003
acA3800-14um USB 3.0 Mono MT9J003
100140 MT9P031
acA1920-25gc GigE Color MT9P031
100141 MT9P031
acA1920-25gm GigE Mono MT9P031
100142 MT9P031
acA1920-25uc USB 3.0 Color MT9P031
100143 MT9P031
acA1920-25um USB 3.0 Mono MT9P031
100144 MT9P031
acA2500-14gc GigE Color MT9P031
100145 MT9P031
acA2500-14gm GigE Mono MT9P031
100146 MT9P031
acA2500-14uc USB 3.0 Color MT9P031
100147 MT9P031
acA2500-14um USB 3.0 Mono MT9P031
100148 MT9P031
daA1920-15um (No-Mount) USB 3.0 Mono MT9P031
100149 MT9P031
daA1920-30uc (S-Mount) USB 3.0 Color MT9P031
100150 MT9P031
daA1920-30um (S-Mount) USB 3.0 Mono MT9P031
100151 MT9P031
daA2500-14lc (S-Mount) BCON for LVDS Color MT9P031
100152 MT9P031
daA2500-14lm (S-Mount) BCON for LVDS Mono MT9P031
100153 MT9P031
daA2500-14uc (S-Mount) USB 3.0 Color MT9P031
100154 MT9P031
daA2500-14um (S-Mount) USB 3.0 Mono MT9P031
100155 MT9P031
daA1920-30um (No-Mount) USB 3.0 Mono MT9P031
100156 MT9P031
daA1920-30um (CS-Mount) USB 3.0 Mono MT9P031
100157 MT9P031
daA1920-30uc (No-Mount) USB 3.0 Color MT9P031
100158 MT9P031
daA1920-30uc (CS-Mount) USB 3.0 Color MT9P031
100159 MT9P031
daA2500-14um (No-Mount) USB 3.0 Mono MT9P031
100160 MT9P031
daA2500-14um (CS-Mount) USB 3.0 Mono MT9P031
100161 MT9P031
daA2500-14uc (No-Mount) USB 3.0 Color MT9P031
100162 MT9P031
daA2500-14uc (CS-Mount) USB 3.0 Color MT9P031
100163 MT9P031
daA2500-14lm (No-Mount) BCON for LVDS Mono MT9P031
100164 MT9P031
daA2500-14lm (CS-Mount) BCON for LVDS Mono MT9P031
100165 MT9P031
daA2500-14lc (No-Mount) BCON for LVDS Color MT9P031
100166 MT9P031
daA2500-14lc (CS-Mount) BCON for LVDS Color MT9P031
100167 MT9P031
puA1920-30uc USB 3.0 Color MT9P031
100168 MT9P031
puA1920-30um USB 3.0 Mono MT9P031
100169 MT9P031
puA2500-14uc USB 3.0 Color MT9P031
100170 MT9P031
puA2500-14um USB 3.0 Mono MT9P031
100171 MT9V022
scA750-60gc GigE Color MT9V022
100172 MT9V022
scA750-60gm GigE Mono MT9V022
100173 PYTHON 1300
acA1300-200uc USB 3.0 Color PYTHON 1300
100174 PYTHON 1300
acA1300-200um USB 3.0 Mono PYTHON 1300
100175 PYTHON 1300
acA1300-75gc GigE Color PYTHON 1300
100176 PYTHON 1300
acA1300-75gm GigE Mono PYTHON 1300
100177 PYTHON 2000
acA1920-150uc USB 3.0 Color PYTHON 2000
100178 PYTHON 2000
acA1920-150um USB 3.0 Mono PYTHON 2000
100179 PYTHON 2000
acA1920-48gc GigE Color PYTHON 2000
100180 PYTHON 2000
acA1920-48gm GigE Mono PYTHON 2000
100181 PYTHON 300
acA640-300gc GigE Color PYTHON 300
100182 PYTHON 300
acA640-300gm GigE Mono PYTHON 300
100183 PYTHON 300
acA640-750uc USB 3.0 Color PYTHON 300
100184 PYTHON 300
acA640-750um USB 3.0 Mono PYTHON 300
100185 PYTHON 500
acA800-200gc GigE Color PYTHON 500
100186 PYTHON 500
acA800-200gm GigE Mono PYTHON 500
100187 PYTHON 500
acA800-510uc USB 3.0 Color PYTHON 500
100188 PYTHON 500
acA800-510um USB 3.0 Mono PYTHON 500
100189 PYTHON 5000
acA2500-20gc GigE Color PYTHON 5000
100190 PYTHON 5000
acA2500-20gm GigE Mono PYTHON 5000
100191 PYTHON 5000
acA2500-60uc USB 3.0 Color PYTHON 5000
100192 PYTHON 5000
acA2500-60um USB 3.0 Mono PYTHON 5000
100193 PYTHON 5000
Basler MED ace 5.3 MP 20 mono GigE Mono PYTHON 5000 Series Production: now
100194 PYTHON 5000
Basler MED ace 5.3 MP 20 color GigE Color PYTHON 5000 Series Production: now

Sorry, there are no results for the selected filters.

Show more