Menu
Application Notes
Silently installing selected pylon features
Document number: AW000846
In this application note, you will learn how to perform a silent installation of the Basler pylon 4 Camera Software Suite. You can either perform a full installation or install selected features only.
When installed silently, the pylon installer will not display messages or windows during its progress.
This document applies to the Basler pylon 4 Camera Software Suite only. For newer pylon versions, refer to the document "pylon Deployment Guide".
The application note explains how to perform the following tasks:
- Silently install selected features using the pylon runtime redistributable packages and msiexec.exe
- Silently install selected features using the pylon Camera Software Suite installer
- Prevent the pylon installation from being displayed in the Add and Remove Software panel
- Silently uninstall pylon