Menu
Product Insights
Increased Cleanness Requirements for Medical & Life Sciences
The Basler MED ace camera series has been specifically designed to meet the needs of medical and life science applications. A special feature of the MED ace cameras is the new Dust Protection Feature Set, which seals the sensor chamber to protect it from dust or dirt particles.
In this Product Insight, Basler Product Manager Dr. Melanie Gräsel explains why special attention should be paid to possible contamination of the optical path in medical and life sciences applications, and describes in detail the functionalities of the Dust Protection Feature Set
- The Dependence on the f-stop
- The Dependence on the Position in the Beam Path
- The Dust Protection Feature Set