Menu
Customer Stories
INCREMO: In-Vehicle Police Car Video Application with Basler IP Cameras
To increase the quality of their service performance, the Czech police equipped their vehicles with video cameras as an integral element of the INCREMO monitoring system. INCREMO provides the police officers with complex text information about individuals and cars as well as video intelligence from the vehicle’s surroundings. The system securely encrypts all collected data and authenticates users before providing access, to ensure that sensitive information remains safe.
Basler IP cameras are an integral element of the Czech Police’s INCREMO video monitoring system. The INCREMO system includes a PC which is adapted to in-vehicle use, a recording device and two Basler IP cameras. The PC is controlled via a touch-screen display and the police radio unit, and provides many preset applications such as information retrieval (checking for a person’s criminal record, for example), or chat and navigation. All installed equipment starts automatically when the vehicle’s engine is turned on. An automatic diagnostic system inside the vehicle monitors the state of the PC, the video recorder, and the battery, as well as the readiness of the radio station. The user-friendly interface on the LCD touch screen allows the police officers on duty to continuously control every piece of equipment.
Practical examples of typical INCREMO operations would be the following:
- A police patrol checking a suspect person, where one police officer verifies the person’s identity on the touch screen in the car.
- In the case of vehicle examination, the police patrol verifies a particular vehicle based on its license plate in order to find out whether it has the necessary technical certificate or if it is has been reported stolen.
- In the event of a car accident, the operation center can be briefed on the current situation through the messaging system – for example to convey a victim’s health status