Menu
Application Notes
How to optimize Basler IP video performance
Document number: AW000844
When a camera is working with its default settings, it automatically tries to find the best values for gain, exposure time, and lens aperture for a "standard" scenario. "Standard" could be regarded as the best compromise for different situations (in terms of brightness, speed of moving objects, etc.).
But this compromise would definitely not be the best fit for all situations.
The application note describes the best settings for different use cases.
The following use cases are explained:
- "Minimize noise" use case
- "Minimize motion blur" use case
- "High frame rate" use case
The application note shows which parameters you have to adapt in order to optimize the video performance for the different use cases.