Menu
Use Case
CoaXPress Solutions for High-Resolution Gene Sequencing
Using the latest gene sequencing methods such as NGS (Next Generation Sequencing), even subtle differences in the structure of the genetic material can be detected and evaluated. In laboratory automation, ever-faster and more reliable methods are being used for this purpose. Image processing enables the manufacturers of sequencing equipment to visualize the small building blocks of life very rapidly and with great accuracy. A system with a CoaXPress 2.0 interface consisting of a camera, interface card or frame grabber and other components is a compelling choice in terms of data throughput and high quality of measurement results.
With other accessories, Basler provides all these components with CoaXPress interface 2.0 for the entire vision system.
Learn more in our Use Case.