Menu
Customer Stories
Basler Cameras Provide Jack Nicklaus Golf Academies with Superior Images
Video analysis is a big part of golf instruction. This technique has been evolving over the years as the naked eye cannot dissect what the human body is doing through the golf swing, not to mention what the club head is doing at 100+ mph. The use of high-speed video is essential for the finest instruction. Nicklaus Academies relies on Basler cameras to provide their customers with the best of the best. Each Jack Nicklaus Coaching Studio contains a minimum of three Basler cameras, and as many as seven, depending on the application and the number of views desired. Up to four cameras collect images in the Full-Swing Instruction Bay while two to three cameras are deployed in the Putting Lab. A custom software program was created specifically to handle the number of frames-per second and the size of the video files. The system is deployed around the world in over 22 academies with an annual growth of four to seven additional locations scheduled for future years.