Menu
Customer Stories
Let It Shine – Automated Optical Inspection of High Gloss Automotive Parts with Helmee AOI and Basler ace L Cameras
After the galvanizing process at most coating companies, inspectors have to perform the difficult task of distinguishing and sorting good versus defective parts. This visual inspection requires bright light to find defects. However, the mirrored surfaces reflect the bright light, making the inspection very difficult for the human eye. The inspection also needs to be very fast. This is why an increasing number of companies are looking for automated processes to perform this highly sophisticated task.
One of these companies is Basler’s customer Helmee Imaging from Finland. The high-tech company develops revolutionary systems for the automated optical inspection (AOI) of parts with shiny or reflective surfaces. The Helmee AOI system consists of three Basler ace L cameras, an industrial PC, two industrial robots, a container transport belt and safety barriers. It automatically lifts the parts from the containers, performs a 100 % visual inspection and sorts the parts according to the inspection results.
In our Success Story "Let It Shine – Automated Optical Inspection of High Gloss Automotive Parts with Helmee AOI and Basler ace L Cameras“, you learn exactly how this system works and why the Basler ace L camera is so well-suited for this application.