Menu
Illumination
The first part of the image processing chain is illumination, and it is one of the most sensitive parts. Investing more money in an optimized illumination system will reduce both programming and image analysis costs. Illumination can be separated into dark and bright field, continuous lights, and flashed lights. Flashed lights are often used with area scan cameras. For line scan cameras, the illumination must be very constant in brightness.
Optimum illumination can be achieved by using different parts of the spectrum or polarization, as well as collimated light, diffuse light, or a mixture of both. A mixture of collimated and diffuse light is often necessary for inspection of metal parts. Typical illumination systems make use of LEDs, halogen lamps, metal halide lamps, lasers, and fluorescent lights with low and high frequencies. Each of these illumination sources has its advantages and disadvantages. The right choice is the key to high quality image capture and accurate image analysis.
Illumination Partners
Advanced Illumination, Inc.
24 Peavine Drive
Rochester, VT 05767
USA
www.advancedillumination.com
Illumination Technologies, Inc.
5 Adler Drive
East Syracuse, NY 13057
USA
www.illuminationtech.com
LAT elektronik AB
Krossgatan 18
SE-16250 Vällingby
Sweden
www.latab.se
Schott Glas
Hattenbergstr. 10
55122 Mainz
Germany
www.schott.com
StockerYale Inc.
32 Hampshire Road
Salem, NH 03079
USA
www.stockeryale.com
Vision Light Tech
Protonenlaan 22
5405 NE UDEN
Niederlande
www.vlt.nl
Volpi AG
Wiesenstrasse 33
8952 Schlieren-Zürich
Switzerland
www.volpi.ch