Menu
Basler SLP Controller - Flexible in Use And Rich in Options
The Basler SLP Controller expands the possibilities for using the Basler SLP concept significantly. The controller is used wherever special demands are made on the lighting of a vision system. It is therefore a useful addition to the concept of the Basler Camera Light series. The Basler SLP Controller can be used to operate most of the various machine vision lightings available as it offers many options that meet the most specific lighting requirements of a vision system.

Basler SLP Controller
The Basler SLP Strobe Controller 121040 allows the easy integration of any light source in a Vision System application by using the Basler SLP feature. The feature enables the direct communication between the Basler SLP Controller and the Basler ace U and L camera, allowing the lighting to be easily operated in different modes such as continuous, strobe or overdrive. When using the Basler SLP Controller, the user can also gain access to the simple lighting concept via a uniform software interface, the pylon Camera Software Suite.
Explore more details about the Basler SLP Controller
Availability of the Basler SLP feature
Want to know when the SLP feature is available on the latest ace U and L cameras?
Find all availabilities here
Don’t want to spend much time on lighting applications?
Achieve results more quickly with the Basler Camera Light vision system setup.
Find out more