Your browser is out of date. It may not display all features of this websites. Learn how to update your browser.

OK
Careers | Investors
12-Feb-2018

The MIPI CSI-2 Interface for Embedded Vision Applications

The MIPI CSI-2 Interface for Embedded Vision Applications

There is an increasing number of embedded vision applications on the market. Embedded vision systems are based on an embedded processing board and a camera module. Such a system can manage vision tasks more affordably and efficiently.

The interface, which is the connection between the camera module and processing board, plays a key role in the setup of such an embedded vision system. The plug and play USB 3.0 interface can be used here, for example. LVDS interfaces are also worth considering, particularly for FPGA-based systems. But in very many cases, the MIPI CSI-2 interface is the best choice.

This White Paper provides an overview of the significance and features of this important interface for the embedded vision field.

Download White Paper

The Document Download area also contains other White Papers on many different fascinating topics, including other topics in the embedded vision field.