Your browser is out of date. It may not display all features of this websites. Learn how to update your browser.

Careers | Investors

New Software Package for Basler ToF Camera – What Are the Benefits?

New Software Package for Basler ToF Camera – What Are the Benefits?

Interest in 3D applications and demand for 3D cameras are on the rise – and the advancement of the Basler ToF Camera is also in full swing. The newly launched software package (Version: 1.2.0) for the Basler ToF Camera includes the following new features:

  • Improvements of the spatial and temporal filters and the outlier suppression, which significantly reduces the noise in the depth data and creates fewer artifacts around moving objects or edges. In this new software package, the filters also achieve a stable state much faster than in the previous version.
  • An extensive Programmer’s Guide for the C++ API
  • a C++ Sample Program for using the camera data in the Point Cloud Library
  • Visual Basic .NET suppot to develop applications
  • .NET improvements in terms of user friendliness and easier development of applications when using .NET combined with the Basler ToF Camera, e.g. a sample program to depict the range map as a bitmap
  • Device Removal Support

The software package is available for the following camera modules and is ready to download on the website:

107002 tof640-20gm_850nm (Revision 07 or newer is recommended)
107002 ES-TOF (Revision 07 or newer is recommended)

This is exclusively a producer update – the camera does not need to be updated to profit from the extensive improvements.