Your browser is out of date. It may not display all features of this websites. Learn how to update your browser.

OK
Careers | Investors
10-Jan-2017

New Additions to the USB 3.0 Card Portfolio

New Additions to the USB 3.0 Card Portfolio

We've expanded our existing USB 3.0 portfolio of accessories to include two new PCI Express USB 3.0 cards with 2 and 4 ports respectively.

The highly efficient 2-port card features two host controllers to ensure that you can run both USB cameras in parallel and at high bandwidth without sacrificing transfer speed. The new 4-port card by contrast offers the opportunity to operate 4 USB cameras simultaneously using distribute bandwidth, a major benefit for keeping overall system costs under control.

An overview of the key features of the two cards:

USB 3.0 Card PCIe, Renesas, 2 HC, x4, 2 Ports

  • 2 ports for use of up to 2 USB cameras
  • 2 host controllers and 4 lanes to the computer for transferring at a high bandwidth of 360 MB/s per camera

USB 3.0 Card PCIe, Fresco FL1100, 1HC, x1, 4 ports

  • 4 ports for use of up to 4 USB cameras
  • 1 host controller and 1 lane to the computer for transferring at a high bandwidth of 380MB/s per camera.