Your browser is out of date. It may not display all features of this websites. Learn how to update your browser.

OK
Careers | Investors
04-Oct-2017

In Series Production: ace U with Sony STARVIS Sensors

In Series Production: ace U with Sony STARVIS Sensors

The series production of eight new ace U models with the IMX178 and IMX226 sensors from Sony's STARVIS line is now starting. They offer resolutions of 6 and 12 megapixels and deliver up to 59 frames per second. The eight new models are the first Basler cameras to feature innovative back-illuminated rolling shutter CMOS sensors. They stand out with their extremely high sensitivity at small pixel sizes of 2.4 µm (IMX178) or 1.85 µm (IMX226). A special aspect of these sensors is the very low dark noise of only three electrons, combined with a quantum efficiency of over 80%. With these particularly light-sensitive sensors, the eight new ace U cameras deliver high image quality even in low light conditions. They also offer an excellent price/performance ratio. This makes the new ace U cameras particularly suitable for applications in the areas of manual light or fluorescence microscopy, as well as in the electronics industry for less complex assembly systems.

All new ace U models are available with the proven GigE or USB 3.0 interface, and conform to GigE Vision 2.0 or the USB3 Vision standard. The GigE models excel with high-performance GigE Vision 2.0 features such as PTP. The ace U color models also include the PGI feature set--the unique combination of 5x5 debayering, color anti-aliasing, denoising and improved sharpness.

Do you already know our Basler Lenses?

To resolve the 1/1.8" and 1/1.7" sensors with small pixel sizes of only 2.4 µm and 1.85 µm requires the right optics. With our Basler Lenses you make the right choice for a variety of applications. Our Basler Sales Team will be happy to advise you on the selection in order to find the solution that suits you best.

The following ace U models are now in series production:

Camera model Resolution (HxV) Frame Rate Mono/Color Interface Sensor
acA3088-57um 3088 px x 2064 px 59 fps Mono USB 3.0 IMX178
acA3088-57uc 3088 px x 2064 px 59 fps Color USB 3.0 IMX178
acA3088-16gc 3088 px x 2064 px 16 fps Color GigE IMX178
acA3088-16gm 3088 px x 2064 px 16 fps Mono GigE IMX178
acA4024-8gm 4024 px x 3036 px 8 fps Mono GigE IMX226
acA4024-29um 4024 px x 3036 px 31 fps Mono USB 3.0 IMX226
acA4024-8gc 4024 px x 3036 px 8 fps Color GigE IMX226
acA4024-29uc 4024 px x 3036 px 31 fps Color USB 3.0 IMX226

For further information, please contact the Basler Sales Team or your local Basler distribution partner.

Didn’t see quite what you need? Discover other models of the ace U line and learn all about the individual ace product lines on our website. Be sure also to have a look at our entire ace portfolio with more than 120 models.