Your browser is out of date. It may not display all features of this websites. Learn how to update your browser.

OK
Careers | Investors
02-Nov-2017

Deep Learning in Action: Vision Sensor “on the Edge” with Amazon Web Services

Deep Learning in Action: Vision Sensor “on the Edge” with Amazon Web Services

How do I develop an embedded vision sensor that detects and unequivocally classifies objects? We have compiled a use case for you with a simple example that shows how you can prepare a Convolutional Neural Network (CNN) for the detection and classification of objects with the help of a deep learning framework and then use this on an embedded device – and all this with only the support of the following components:

The Basler dart daA2500-14uc camera module used here is available not just as an individual camera but also as a dart USB Evaluation Kit, in which the required camera accessories such as lens and USB cable are already included. All you need to do is connect the camera module to a processing board, then you can start programming your embedded vision solution.

Download use case now