Your browser is out of date. It may not display all features of this websites. Learn how to update your browser.

OK
Careers | Investors
11-Apr-2018

Critical Links Development Kit with dart BCON for LVDS Receives Vision System Design Innovators Award

Critical Links Development Kit with dart BCON for LVDS Receives Vision System Design Innovators Award

The magazine Vision Systems Design is now announcing the fourth Innovators Awards, celebrating innovative technologies and products in the machine vision industry. With its Embedded Vision Development Kit for the dart BCON for LVDS, Critical Link impressed the jury, winning the bronze Innovators Award. The prize was awarded during the Vision Show in Boston.

The MitySOM-5CSx Embedded Vision Development Kit (VDK) is a complete hardware and software reference design for the Basler dart BCON for LVDS camera modules. It is based on the industry-suitable MitySOM-5CSx system-on-module from Critical Link, which has an Intel PSG/Altera Cyclone V SoC processor. The MitySOM-5CSx baseboard offers up to two BCON for LVDS interfaces, along with a series of additional communication interfaces and expansion options. The kit is available in two variants: a single-camera package with a 5 MP dart BCON for LVDS (daA2500-14lc) and a stereo camera package with two dart BCON for LVDS (daA1280-54lm).

The Development Kit offers the option of streaming images via the user-friendly Basler pylon Camera Software Suite or putting them out directly via the FPGA and the available HDMI interface. In both cases, pylon is also used to configure the camera modules.

The Embedded Vision Development Kit from Critical Link impresses not only with technical details but also its long-term availability and a design that is suitable for industrial use.

Critical Link is an engineering company for embedded systems. It has substantial experience in FPGA programming and the development of electronic systems for a wide range of applications.

For more information about Basler's portfolio for embedded vision, please visit www.baslerweb.com/embedded. You can find more information about Critical Link’s MitySOM-5CSx Embedded Vision Development Kit (VDK) for Basler dart here: https://www.baslerweb.com/en/embedded-vision/referenz-designs/critical-link-mitysom-5csx-development-kit/