Your browser is out of date. It may not display all features of this websites. Learn how to update your browser.

OK
Careers | Investors
02-Nov-2017

1" Camera System: Advantages and Recommendations

1

Sensors with higher resolutions are increasingly popular and a good choice for a number of applications in industrial image processing. The latest 1" sensors often provide higher image quality along with faster speed at the same or even increased pixel sizes. This means that an application can record a higher resolution with an unchanged pixel size and high sensitivity and improve the image quality and speed with the help of a 1" sensor. A higher flow-rate cuts costs while increased detection rates yield higher quality.

It’s important to look at these sensors’ format very closely. If you switch from a 1/3" or 2/3" to a 1" camera system, for example, this might not only change the sensor size and corresponding image circle but also have an effect on the working distance. To prevent a reduction in the image quality, the lens should be coordinated with the sensor size. The Basler Lens Selector provides valuable help with the necessary calculations.

This Product Insight uses an example in surface inspection to show the differences between a PYTHON 5000 CMOS sensor by ON Semiconductor and an ICX625 CCD sensor from Sony with the aid of EMVA data and comparative images. You can also find recommendations on what you should consider in regards to suitable optics when switching to a 1" setup and what kinds of 1" lenses the Basler portfolio can offer you.

Read it now!

You can find many additional product insights and white papers on numerous subjects in industrial image processing in the Document Download area. Have a look!