Your browser is out of date. It may not display all features of this websites. Learn how to update your browser.

OK
Careers | Investors
08-Aug-2017

Basler ace L Enters Series Production

Basler ace L Enters Series Production

Basler is starting the series production for all models in its new ace L product line. This expansion of the ace series includes twelve new cameras with the high-resolution CMOS sensors of the latest generation from Sony’s Pregius line.

The twelve new ace L models offer resolutions of 9 and 12 megapixels and frame rates of up to 40 fps. Featuring the high-performance IMX253, IMX255, IMX267 and IMX304 sensors, they stand out for the famously brilliant Pregius image quality with a dynamic range of more than 70 dB and a high quantum efficiency over a broad spectrum of visible light into the NIR. Thanks to these properties, the cameras are also an excellent choice for highly demanding applications.
This includes, for example, high-resolution AOI systems for display inspection or enforcement systems in the ITS market.

In addition to their high image quality and an excellent price/performance ratio, the twelve ace L models stand out with their compact design size, which has a footprint of 30 mm x 40 mm to accommodate the new large-format sensors and thus ensures a simple integration.

All new ace L models are available with the proven GigE or USB 3.0 interface, and conform to GigE Vision 2.0 or the USB3 Vision standard. The GigE models excel with high-performance GigE Vision 2.0 features such as PTP. The ace L color models also include the unique PGI Feature Set for in-camera image optimization.

The twelve ace L models supplement Basler’s product range with additional high resolutions in the C mount portfolio while using a global shutter with a pixel size of 3.45µm. Basler’s new 1-inch lenses are a perfect fit for these sensors. Integration of the cameras is simple and quick using the pylon Camera Software Suite from Basler.

The following camera models are entering series production:

Camera Models Sensor Frame Rate Resolution Mono/ Color Interface
acA4112-8gm IMX304 8 fps 12 MP Mono GigE
acA4112-8gc IMX304 8 fps 12 MP Color GigE
acA4112-20um IMX304 20 fps 12 MP Mono USB3.0
acA4112-20uc IMX304 20 fps 12 MP Color USB3.0
acA4112-30um IMX253 30 fps 12 MP Mono USB3.0
acA4112-30uc IMX253 30 fps 12 MP Color USB3.0
acA4096-11gm IMX267 11 fps 9 MP Mono GigE
acA4096-11gc IMX267 11 fps 9 MP Color GigE
acA4096-30um IMX267 30 fps 9 MP Mono USB3.0
acA4096-30uc IMX267 30 fps 9 MP Color USB3.0
acA4096-40um IMX255 40 fps 9 MP Mono USB3.0
acA4096-40uc IMX255 40 fps 9 MP Color USB3.0

Didn't see quite what you need? Take a look at our entire ace portfolio encompassing over 120 models: www.baslerweb.com/ace

Would you like to learn more about the ace L cameras?

Visit our website at www.baslerweb.com/new-ace or contact the Basler Sales Team or your regional Basler sales partner for more information.

At www.baslerweb.com/ace-product-lines you will find an overview of all product lines in the successful Basler ace series.