Your browser is out of date. It may not display all features of this websites. Learn how to update your browser.

OK
News / Press | Careers | Investors Webshop

Embedded Vision Solutions as Smart Sensors for IoT Applications

Our live demo shows how an embedded vision solution can be used as an efficient and intelligent sensor for image data classification. Read more about it.

Here is how it Works

IoT sensors, such as a camera, are usually only connected to the cloud with very low bandwidth. Therefore the transmission of the large amount of image data would be slow. One solution approach is to perform the analysis of the image data at the location of the camera sensor itself, "on the edge" (Processing on the Edge), and then only transfer the evaluated data to the cloud. A connection with a very low bandwidth is completely sufficient for this purpose. Accordingly, the transfer to the cloud can be carried out very quickly and the camera can react to an incident.

More on our embedded vision solutions Download the complete Use Case now

Step 1: Choose the Right Hardware

This live demo is based on the award-winning Basler Embedded Vision Kit. This kit consists of

  • a dart BCON for MIPI camera module by Basler
  • a 96 Boards™ compatible processing board with Qualcomm® Snapdragon™ SoC and
  • a 96 Boards™ compatible mezzanine board to directly connect the camera module to the processing board

This solution allows image data captured by the camera module at high frame rates to be processed directly on the processing board.

Discover our Embedded Vision Portfolio

Step 2: Train neural networks

The aim of the live demo is to be able to classify different Lego figures (craftsman, astronaut, cook etc.) or different traffic signs. This task is performed by neural networks, more precisely by Convolutional Neural Networks (CNNs).

Basler initially trained two different CNNs, one for the classification of Lego figures, the other for the classification of traffic signs. The trained CNNs are not very large with only a few megabytes and can be transferred from the cloud to the edge device in an acceptable amount of time via a low-bandwidth connection. After transferring the Lego figure CNN, the Edge Device was able to reliably classify the figures and report the result to the cloud with low bandwidth requirements and low latency. To "retool" the Edge Device to classify traffic signs, only the corresponding traffic sign CNN had to be transmitted from the cloud, so that the smart sensor was then able to reliably detect different traffic signs.

To the software for embedded vision

The Advantages at a Glance

  • low bandwidth requirements for linking the sensor to the cloud
  • low latency in the reaction of a cloud application to a sensor event
  • ideal opportunity for simultaneous “remote maintenance” of multiple sensors OTA (sensor configuration, firmware update or e.g. uploading a new CNN for a new classification task)

Do you have any more Questions? We are happy to help.

Do you have questions about this solution, your individual solution or our products?

Contact our Sales Team

Back to Webshop