Embedded Software
System Image for NVIDIA®’s Jetson Nano Developer Board
Version: 1.0.0
Operating System: Linux ARM
To start up Basler‘s 5 and 13 MP MIPI/CSI-2 cameras with an NVIDIA Jetson Nano developer board you’ll need this system image and a microSD card with a capacity of at least 16 GB. You need to flash the image onto the SD card using common image flashing tools and insert the card into the microSD card slot on the Jetson Nano Board. The subsequent system start-up is described in detail on one of the following pages, depending on which kit you have:
https://docs.baslerweb.com/daa4200-30mci-jnano-nvdk https://docs.baslerweb.com/daa2500-60mci-nvjet-nvdk-addon https://docs.baslerweb.com/daa4200-30mci-nvjet-nvdk-addon