Manuals
Installation and Setup Guide for Cameras Used with pylon for Windows
The Installation and Setup Guide for Cameras Used with pylon for Windows (Software version 6.x) provides valuable information that should be taken into account prior to installation and setup of the pylon 6 Camera Software Suite on a Windows PC. The document explains all necessary steps for a successful pylon installation on a Windows host system. It also provides details on important measures for optimizing the data throughput for the Basler camera based on the specific camera interface (such as GigE Vision, USB3 Vision). Finally, this document describes the first steps for successfully setting up a Basler camera.
Basler strongly recommends reading the Installation and Setup Guide for Cameras Used with pylon for Windows in its entirety prior to installing the pylon 6 Camera Software Suite and ensuring that its suggestions are followed when using pylon, especially during software development.