Application Notes
How to build pylon applications on Raspberry Pi
This application note explains how pylon applications can be built on a Raspberry Pi ARM board.
The procedures described assume you are using the following hardware and software components:
- Raspberry Pi 4
- Raspbian operating system
- Windows 10 (32-bit or 64-bit) PC
- pylon 6.1 Camera Software Suite installed on the Windows PC
- Basler GigE Vision camera or Basler USB camera
In a step-by-step tutorial, you will learn how to:
- Configure the Basler GigE Vision or USB camera for use on a Raspberry Pi
- Establish a connection between the Basler GigE Vision or USB camera and the Raspberry Pi
- Install the pylon for Linux ARM package
- Build and run pylon ARM applications directly on the Raspberry Pi board
- Grab your first images using the Raspberry Pi and a connected Basler GigE Vision or USB camera