Application Notes
Comparison of Basler BCON for LVDS interface and Camera Link interface
Document number: AW001394
Basler offers both Camera Link and board level cameras with BCON for LVDS, Basler's interface for embedded vision applications.
This document compares the two interfaces. They are notably similar in terms of data transmission and protocol, as BCON for LVDS has inherited many properties of the Camera Link interface and is in many ways Camera Link's 'little brother'. Even so, the BCON interface also has other features of interest, especially if the interface is being used for embedded vision applications.
Other important points that come into play when comparing the interfaces and described in this document are:
- Data transfer methods for each interface
- Cabling and hardware connection
- Camera configuration
- Image capture, and
- Working with the pylon Camera Software Suite