Product Insights
Basler Accessories for Stable USB 3.0 Systems: These are the Components You Need
A vision system is built up of various components, including camera, lens and light source. To create a stable system, you‘ll need suitable accessories, such as a cable, chip set or host adapter.
At Basler, our Product Qualification department is responsible for verifying the compatibility of accessories with our cameras. Components such as cables, host adapters, chipsets and motherboards are run through a full set of checks and diagnostics. This way we can be certain that accessories we have approved as compatible with our cameras actually deliver optimal performance for the whole set-up.
A USB 3.0 camera system will only be stable and deliver optimal performance if all components are compatible and harmonized to work together. Learn more about Basler‘s recommendations on accessories for stable USB 3.0 camera systems in this Product Insight. On top of that, we will show you which factors you should take into consideration when selecting components with our convenient 10-point plan.