Vignetting Correction - New Basler Feature Corrects Edge Shadowing
Optimized Image Quality and Cost Reduction with the New "Vignetting Correction" Feature from Basler
With "Vignetting Correction" we extend the image processing options of our ace U and ace L product lines with a feature that enables the correction of edge shadowing.
Vignetting is a well-known phenomenon in image processing and describes the decrease in image brightness towards the edge. If the image circle of the lens used is too small in relation to the camera sensor, this effect can manifest strongly and affect the image quality accordingly. Details at the edge of the sensor are often difficult or impossible to inspect. The inspection is made more difficult by the different brightness values across the image. In many cases the choice of a larger lens - for example from 2/3" to 1" - can help, but this solution is usually associated with higher costs.
Vignetting Correction is a patent-pending feature from Basler that corrects the described unwanted effect in a unique way, thereby enabling cost savings when combining cameras and lenses. After a one-time calibration of the camera, there are no negative effects on frame rate or image quality as the correction values are stored in the camera and automatically taken into account in the image output. Thus, for example, users can combine ace cameras with Sony IMX304 or IMX253 1.1" format sensors with 1" lenses without having to accept any edge shadows. It is no longer necessary to switch to a lens with a larger image circle.
The Vignetting Correction feature is available for selected ace U and ace L models with GigE and USB 3.0 interfaces.
For more information and an overview of attractively priced combinations of Basler cameras and lenses with Vignetting Correction, please visit www.baslerweb.com/new-ace-features
Your request cart is currently empty. Please add at least one product to send a quote request. If you would like to send a message directly to our sales team, please use this form.