Series Production Started: Four New ace U Models with the IMX287 and IMX273 Sensors from Sony
The four new ace U USB 3.0 models feature resolutions of VGA and 1.6 megapixels and have now moved into series production. They are equipped with the IMX287 and IMX273 sensors from Sony's Pregius series and deliver up to 525 frames per second.
The IMX273 sensor offers the well-known outstanding Pregius image quality, high speeds and low noise. The IMX287 sensor, on the other hand, has twice the pixel size with an edge length of 6.9 µm. This results in an increased saturation capacity and a higher dynamic range with the same sensitivity and also low noise.
Both sensors feature the Ultra Short Exposure Time Mode, which enables extremely short exposure times of up to one microsecond (1 µs). This makes the cameras particularly attractive for applications with fast movement, such as in the print sector.
With their features, the four ace U models are also ideally suited as upgrades for CCD cameras with low resolutions.
The four new ace U USB 3.0 cameras include the feature set PGI, a unique combination of 5x5 debayering, color-anti-aliasing, denoising and improved sharpness.
Didn’t see quite what you need? Discover other models of the ace U line and learn all about the individual ace product lines on our website. Be sure also to have a look at our entire ace portfolio with more than 130 models.
Your request cart is currently empty. Please add at least one product to send a quote request. If you would like to send a message directly to our sales team, please use this form.