Cable length | Straight USB 3.0 data cable with screw connection | Angled USB 3.0 data cable with screw connection |
---|---|---|
1m | 2200000204 | 2000036369 |
3m | 2000033239 | 2000035994 |
5m | 2000033241 | 2000035995 |
8m | 2000034891 | ̶ |
The optical changes are rather inconspicuous – a thinner and thus more flexible raw cable, more compact plugs and a small logo make the industrial cable more visually appealing.
In the long term, however, the cable design excels particularly on a functional basis. A lower voltage drop, reduced signal attenuation and higher immunity of the cable against interferences increase the application’s safety. This is due to more generously sized cables, the selection of the right core material and the combination with the most suitable core diameter.
With this step, Basler is ensuring that its own data cable portfolio continues to be state-of-the-art and will significantly improve confidence in long USB 3.0 data transfers.
* USB 3.0 and USB 3.1 Gen 1 refer to exactly the same standard.For simplicity's sake, we will use the term USB 3.0 below.