Have You Already Updated Your Basler pylon USB 3.0 AIK Adapter?
The Basler pylon USB 3.0 AIK adapter allows you to operate Basler USB 3.0 cameras using Cognex VisionPro. After a few simple configuration steps, the Basler USB 3.0 cameras appear in VisionPro for further configuration as desired. The new version 5.0 of the AIK adapter uses pylon 5 to connect with our Basler cameras. You'll benefit from the new GenICam
3 technology which significantly accelerates the camera triggering, all while requiring significantly less storage space.
The Basler pylon USB 3.0 AIK adapter can be downloaded for free from our download area
. We've included an Application Note
to help with the installation and setup of the driver.
Once the pylon Camera Software Suite or pylon Runtime (U3V) has been installed, the AIK adapter will run on all 32 or 64-bit operating systems.
Your request cart is currently empty. Please add at least one product to send a quote request. If you would like to send a message directly to our sales team, please use this form.