It is nearly impossible to distinguish an object’s texture from the surface properties in a single image. With the photometric stereo approach, at least three and usually four images are taken with a camera where the object is illuminated from different directions. Four images (texture, X- and Y-derivation and average curvature) are typically calculated from these captures. This separation of the surface properties from the texture enables a clean evaluation of the products.
Due to the time-consuming calculation in the CPU the required cycle times in production cannot usually be met. MSTVision GmbH, a development service provider for tailor-made solutions in the field of industrial image processing, has used a frame grabber in its photometric stereo approach and was thus able to significantly accelerate the implementation of image acquisition and calculation in the process.
Your request cart is currently empty. Please add at least one product to send a quote request. If you would like to send a message directly to our sales team, please use this form.