Dust Protection – A New Feature Set for the Basler MED ace
Does your Medical & Life Sciences application have particularly high cleanliness standards for cameras? Four of our Basler MED ace models are now available with the MED Feature Set Dust Protection. And what is especially important – even with this improvement, we’re keeping the price of the four models stable.
We designed the Basler MED ace camera series specifically for the Medical & Life Sciences field. We are now enhancing the first four models with the new MED Feature Set Dust Protection
. All USB 3.0 color cameras with 2.3 MP and 5.1 MP will now offer the new Feature Set. With Dust Protection, Basler combines four components that meet the special cleanliness standards often required of cameras by Medical & Life Science applications: Sealing of the sensor room, cleanroom production, strict inspection for dust and other particles as well as high robustness during daily use. And the best part – even with this improvement, we’re keeping the price of the four models stable.
The Basler MED Feature Sets
are part of the Basler MED ace cameras. The Dust Protection Feature Set supplements the series of existing MED Feature Sets, which includes Easy Compliance, Brilliant Image, Perfect Color, Low Light Imaging, Industrial Excellence and High Speed. The sophisticated requirements which Basler configured specifically for the Medical & Life Sciences areas combine hardware, firmware and software functions. Their great benefit lies in helping customers reduce their development effort. They enable top-quality images in minimal time, while also offering full flexibility for individual requirements.
The color and monochrome cameras in the Basler MED ace series
stand out not only with their MED Feature Sets but also with the latest CMOS sensors in the Pregius line from Sony, or the PYTHON line from ON Semiconductor. They achieve up to 164 frames per second and have a resolution up to 20 MP. The certification of the quality management system under ISO 13485:2016 is particularly valuable for clients using the cameras in Medical & Life Science applications. Basler thus offers additional and higher quality standards for the production, distribution and service of digital cameras.
Would you like to learn more about the Basler MED ace cameras and the different MED feature sets? Contact us! If you have questions or need support, our Sales Team
is pleased to help you at any time.
Your request cart is currently empty. Please add at least one product to send a quote request. If you would like to send a message directly to our sales team, please use this form.