CoaXPress 2.0 as an Alternative to Camera Link - More Performance and Lower System Costs When Changing the Camera Interface
In the field of industrial image processing, two interfaces dominate in demanding applications that require a frame grabber or an interface card: Camera Link and CoaXPress 2.0. The two interfaces are technologically very similar. However, switching from Camera Link to CoaXPress 2.0 is often advantageous. With CoaXPress 2.0, for example, longer cable lengths can be used and a higher bandwidth can also be achieved. Here CoaXPress 2.0 offers many possibilities to optimize the existing Camera Link system and will prepare you for higher system requirements in the future.
This White Paper explains in detail the arguments in favour of switching from Camera Link to CXP 2.0 and the advantages that result from this.
Your request cart is currently empty. Please add at least one product to send a quote request. If you would like to send a message directly to our sales team, please use this form.