Your browser is out of date. It may not display all features of this websites. Learn how to update your browser.

OK
Start configuring your vision system now Webshop
25-Mar-2020

Clinically Clean: Dust Protection for MED ace

Clinically Clean: Dust Protection for MED ace

In order to investigate the smallest structures, medical or scientific imaging laboratories often use microscopic methods with optical magnifications. Particles in the optical path, for example on the sensor glass, can have a disturbing effect depending on the aperture and the associated f-stop numbers and can significantly impair the evaluation of the image information. To prevent such contamination, Basler has developed the Dust Protection Feature Set for selected models of its MED ace camera series.

In her Product Insight "Image Quality in Medical & Life Sciences: Influence of Particles in the Optical Path", Basler Product Manager Dr. Melanie Gräsel explains the interrelationships and effects of contamination as a function of f-stop number and position in the optical path with the help of comparative illustrations and clearly describes how the new Dust Protection Feature Set works.

Download Product Insight now

The Basler MED ace has been specifically designed to meet the needs of medical & life science applications. Learn more about the advantages and special features of this camera series and the MED feature sets designed specifically for it. If you have any questions, please do not hesitate to contact our sales team .

You have questions?
We have the answers!

Our Sales and Technical Support experts are avaiable to advise you on all aspects of Basler computer vision components and solutions.

Contact us

Back to Webshop