Glossary
1080p
1080p is short form term designating a set of HDTV characterized by 1080 horizontal lines resolution and progressive scan.
more
720p
720p describes the lowest resolution defined in the television standard for High Definition TV.
more
ADC
An electronic device that converts a voltage to a proportional digital number.
more
Analog-to-digital converter
An electronic device that converts a voltage to a proportional digital number.
more
AOI
Area of Interest (AOI) - a portion on the camera's sensor.
more
AOI-Level 1
Support of certain resolutions (e.g. CIF, PAL etc.).
more
AOI-Level 2
Support of any resolution, configuration via WebInterface only.
more
AOI-Level 3
Support of any resolution, configuration via WebInterface or video management software.
more
AOI-Level 4
Support of digital pan/tilt by moving an AOI.
more
AOI-Level 5
Support of output scaling configuration via video management software.
more
API
Application Programming Interface (API) - a set of specifications allowing application software to communicate with the camera.
more
Application Programming Interface
Application Programming Interface (API) - a set of specifications allowing application software to communicate with the camera.
more
Area of Interest
A portion on the camera's sensor.
more
Area Scan Camera
Area Scan cameras contain a rectangular sensor with more than one line of pixels, which are exposed simultaneously.
more
Bayer pattern
A regular array of red, green and blue color filters covering a sensor's pixels.
more
Binning
Technique of summarizing several neighboring pixels in the CCD sensor of an industrial camera to a block of pixels with the goal of improving the signal to noise ratio.
more
Blooming
An artifact occurring in images that were acquired by a CCD image sensor.
more
C-Mount
A lens mount for screw in lenses.
more
Camera Link
Camera Link (CL) is a serial communication protocol designed for computer vision applications.
more
CCD
A charge-coupled device (CCD) is a device for movement of electrical charge.
more
CCD Sensor
Electronic device to convert light (photons) into electronic signals (electrons).
more
CCT+
The Basler Camera Configuration Tool Plus (CCT+) is a Windows based tool for configuring Basler cameras that adhere to the Camera Link standard.
more
Charge-Coupled Device
A charge-coupled device (CCD) is a device for movement of electrical charge.
more
CMOS
Complementary metal-oxide-semiconductor (CMOS) is a technology for constructing integrated circuits.
more
CMOS Sensor
Electronic device to convert light (photons) into electronic signals (electrons).
more
Color Creation
Color filter
Colored transparent cover for a pixel.
more
Color Interpolation
Refers to the method of calculating full color information for a pixel.
more
CS-Mount
A lens mount for screw in lenses.
more
Day/Night Functionality
DNS
Domain Name System
more
Dynamic Range
Dynamic Range describes the ratio of the largest signal to the smallest signal (that can be distinguished from noise) in an image.
more
EMVA
The European Machine Vision Association (EMVA) is an association of companies and corporations involved in machine vision and standardization in that field.
more
EMVA1288
The EMVA1288 standard describes a unified method to measure, compute, and present the specification parameters for cameras and image sensors used in machine vision applications.
more
Ethernet
Ethernet is a family of computer networking technologies for local area networks (LANs) commercially introduced in 1980.
more
European Machine Vision Association
The European Machine Vision Association (EMVA) is an association of companies and corporations involved in machine vision and standardization in that field.
more
F-Mount
A bayonet type lens mount.
more
Fixed Box Camera
Fixed camera e.g. for video surveillance.
more
Fixed Dome Camera
Fixed camera with dome housing.
more
FPS
Unit of the frame rate.
more
Frame Grabber
An electronic device installed in a PC for interfacing to a camera.
more
Frame Rate
The number of frames per second that are acquired or transmitted.
more
Frames per Second
Unit of the frame rate.
more
Full HD
A set of HDTV characterized by 1080 horizontal lines resolution and progressive scan.
more
Full well capacity
This quantity refers to the largest charge that a pixel can hold before an overflow of charge into adjacent pixels within the sensor causes the so-called blooming.
more
GenApi
An API for configuring machine vision cameras
more
GenICam™
GenICam is a standard of the European Machine Vision Association (EMVA) allowing to control machine vision cameras via a generic programming interface.
more
GenTL
A module of GenICam providing a unified mechanism for grabbing and streaming images from the camera.
more
Gigabit Ethernet
Gigabit Ethernet (GigE) defines a tethered protocol for data transfer based on the widespread Ethernet standard.
more
H.264
Standard for video compression.
more
HD
The lowest resolution defined in the television standard for High Definition TV.
more
High Profile
A specific H.264 profile.
more
Image Sensor
An electronic device containing a large number of small light sensitive areas (pixels), where photons generate electric charges that are transformed to an electric signal.
more
Interlaced scan
Readout of an image sensor or update of an image frame occurs in an alternating fashion for odd-numbered and even-numbered horizontal lines of pixels.
more
Internet Protocol
The Internet Protocol (IP) is the principal communications protocol used for relaying datagrams (packets) across an internetwork using the Internet Protocol Suite.
more
Internet Protocol address
Unique address in a network.
more
IR-cut filter
An infrared cut filter (IR-cut filter) is used to block light with wavelengths longer than visible light while transmitting visible light.
more
Line Scan
Line Scan cameras have a sensor consisting of 1 to 3 pixel lines.
more
Multi-Streaming and Multi-Encoding
Multicast
Multicasting allows an IP camera to simultaneously transmit images to multiple devices attached to the network.
more
OEM
An original equipment manufacturer (OEM) manufactures products or components.
more
Original Equipment Manufacturer
An original equipment manufacturer (OEM) manufactures products or components.
more
PoE
Power over Ethernet or PoE technology describes a system to pass low voltage electrical power safely, along with data, on Ethernet cabling.
more
Power over Ethernet
Power over Ethernet or PoE technology describes a system to pass low voltage electrical power safely, along with data, on Ethernet cabling.
more
Primary Colors
A set colors from which other colors can be derived.
more
pylon
Basler pylon offers stable, reliable, flexible image data exchange between Basler cameras and PCs at a very low CPU load.
more
RoHs
Collective term for Directive (European Union) 2002/95/EG and its realization into national right.
more
SDK
Software Development Kit
more
Sensor
An electronic device containing a large number of small light sensitive areas (pixels), where photons generate electric charges that are transformed to an electric signal.
more
Signal-to-Noise Ratio
A measure that compares the level of a desired signal to the level of background noise.
more
TCP
Transmission Control Protocol
more
UDP
User Datagram Protocol
more
Unicast
Unicasting is the common capability that lets an IP camera transmit images directly to a single device attached to the network.
more
Vandal resistance
Ability to withstand deliberate attempts of damage.
more
VBR
Variable Bit Rate
more
VGA
A graphics card driver standard.
more
Video Graphics Array
A graphics card driver standard.
more
VoIP
Voice over IP
more
White Balance
The white balance helps to adjust a color camera to the ligting conditions.
more