Basler line scan camera close view

Frame Rate Calculator

Let the Frame Rate Calculator Do the Math!

The Basler Frame Rate Calculator calculates the frame rate or line scan rate for your Basler area scan camera or line scan camera once a few parameters have been specified. For instance, should you wish to define an area of interest (AOI), the tool determines the maximum frame rate or line scan rate that can be achieved.
To run the Basler Frame Rate Calculator use either the Internet Explorer (e.g. IE11) or the Firefox browser. Microsoft Edge and Google Chrome do not support Java plugins and thus the Basler Frame Rate Calculator.

If the applet does not start, please download the latest Java SE Runtime Environment (JRE) Update here: http://java.sun.com/javase/downloads/index.jsp
Deleting the Java cache might be needed in case that already cached Java applications or Java applets such as Basler’s Frame Rate Calculator are preventing a given Java application or applet from running any longer. If you want to know how you can delete your Java cache read our Application Note "How do I delete the Java cache on Windows 7".
Offline version
If you have problems to run the Frame Rate Calculator in your browser, you can also download the following offline version:

Camera Quick Finder

Find Product
 
Please activate cookies in order to download files without having to fill in your data again the next time you visit.