PGI Feature Set

PGI Video

Our video includes a side-by-side image comparison to show you just how our in-camera image optimization PGI gets the optimum out of your images.

Watch the video now

Basler's new proprietary feature set: PGI

Several of our newest camera models come with our powerful in-camera image optimization technology already built in: The proprietary PGI feature set enhances your images at the full speed of your camera. PGI is comprised of a unique combination of 5x5 debayering, color-anti-aliasing, denoising and improved sharpness.
With PGI, your camera will produce better images than ever, without putting additional load on your processor. The PGI feature set is available in dart and pulse color cameras and in all ace color camera models with sensors from the Sony Pregius series or PYTHON sensors from ON Semiconductor.

Harness the full power of pylon and activate the PGI features or change the settings for individual PGI components until you've achieved the optimal results.

The following cameras possess the PGI feature set:

Details on PGI

PGI is comprised of a combination of various features. Learn here about the individual features of PGI.

5x5 Debayering

The term debayering generally describes an algorithm that calculates the color image from the image sensor data. However, as the image sensor does not provide color values for each color in each individual pixel, the algorithm must interpolate to determine that information. Cameras typically offer 2x2 debayering, whereby the two closest pixels are used to calculate the actual color of the image. This can lead in some cases to uneven edges between colors and other artifacts. The 5x5 debayering used in the PGI feature set delivers cleaner transitions between colors and eliminates artifacts altogether.
At the same time, the optimized debayering also assists with noise suppression.

Read more here about PGI in our White Paper.

Color-Anti-Aliasing

Due to the limits of camera resolution, the use of the debayering algorithms can easily lead to color distortion in the captured images. In practical terms, even colorless structures suddenly appear to have color. The aforementioned resolution limits allow color cameras using debayering to capture only specific colors, which in turn produces false interpolation values. PGI uses an expanded informational range during debayering while also simultaneously correcting the incorrect colors.

Denoising

Noise is a phenomenon that occurs in all cameras, and arises from a variety of causes (photon shot noise, sensor noise). Color cameras must not only deal with gray noise but also with color noise caused and reinforced by the sequencing of multiple calculation steps and interpolation. PGI accounts for and avoids this type of noise formation from the start through careful linking and parallelization of calculation operations. In addition, active noise filtering can be applied to further reduce the noise level, which in turn further enhances the image.

Improved Sharpness

Color cameras often struggle to depict particularly fine or sharp structures. The results are aliasing effects or reduced image sharpness. This can be traced back to the interpolation algorithms, known as debayering for cameras with Bayer pattern. Because its interpolation algorithm is adapted for the image structure, the PGI feature set delivers significantly improved sharpness, with the option to pursue further improvement via a supplemental sharpness factor. These enhancements are particularly helpful for applications requiring strong sharpness, such as applications using color cameras to detect and process letters and numbers (such as ANPR for traffic applications) or other fine or sharp-edged structures (such as barcodes).

Still have questions?

Please feel free to contact us with any questions related to the new PGI features set. Talk to us!
*
*
*
*
*

White Paper – PGI

PGI White Paper
Better Image Quality with Basler PGI

We’d Be Glad to Help You

Have a question about our products for your application?
Talk to us!