March 23, 2012

              Visit us at The Vision Show in Boston from May 8-10, 2012

              At the Boston Vision Show, Basler will present its extensive area and line scan camera portfolio. Highlights will be the latest ace area scan camera models and the new line scan camera racer series. Both the ace and the racer series combine great image quality, speed, and a host of useful features with extremely attractive pricing.
              New ace GigE Models with Sony CCD Sensors ICX 414 and ICX415
              • acA645-100gm/gc models fitted with Sony CCD sensors ICX 414 – frame rate: 100 fps at VGA resolution
              • acA780-75gm/gc models fitted with Sony ICX 415 sensors – frame rate: 75 fps at CCIR resolution
              • Ideal for analog camera replacement: same sensors, same footprint, similar price, but way more features
              New Line Scan Camera series – Basler racer
              • Latest line scan sensors based on highly sensitive CMOS technology
              • Line rates of up to 48 kHz via Gigabit Ethernet and up to 80 kHz with the Camera Link interface
              • Available with either a GigE or a camera link interface
              • Present at the show: 2k and 4k models
              • Models with higher resolutions will be introduced at the end of 2012

              Where and When?

              Hynes Convention Center, Boston, USA
              May 8-10, 2012 (Tuesday to Thursday)
              Booth #516

                RSS Feed

                Subscribe the Basler News RSS Feed and get the latest news stories directly delivered to you.
                RSS News Feed
                Please activate cookies in order to download files without having to fill in your data again the next time you visit.